HAB version on iMX8M mini

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HAB version on iMX8M mini

Jump to solution
2,246 Views
antonio_santagi
Contributor IV

Hello,

I read on the HAB code signing Tool User's guide that there are 3 different versions of HAB, HAB3 , HAB4 and AHAB.

I cannot see clearly on the iMX8M mini manuals which version is on this processor.

Which it the HAB ( or AHAB ) version in use on iMx8M mini ?

thank you

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,175 Views
igorpadykov
NXP Employee
NXP Employee

Hi Antonio

iMx8M mini uses HAB4.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,176 Views
igorpadykov
NXP Employee
NXP Employee

Hi Antonio

iMx8M mini uses HAB4.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply