HAB verify boot scripts and other binary data

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HAB verify boot scripts and other binary data

1,582件の閲覧回数
paul_holmquist
Contributor II

Is it possible to use the HAB interface to verify signature of non-image data such as boot-script?  I noticed this being referenced in the Digi board ccimx6sbc UBoot code to check signature of a boot-script using HAB interface before running it.  I'd also like to verify other binary data that I would sign using same PKI tree for images.

Seems like all I would need to do would be to perform all the padding and add a fake IVT data region before signing it using the CST tool (similar to how a kernel image gets signed).  The IVT can be fake since I'm not expecting to execute as an image (calling the HAB ROM interface directly, hab_rvt::authenticate_image()).

Thanks.

ラベル(1)
0 件の賞賛
返信
1 返信

1,479件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

  Yes, it is possible

 

  Look at section 3.4 (Authenticate Image) of "HAB4_API.pdf" in documentation

of CST 3.1.0 package.

https://www.nxp.com/webapp/Download?colCode=IMX_CST_TOOL

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 件の賞賛
返信