HAB i.MX6UL kernel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HAB i.MX6UL kernel

1,307 Views
PramodKumar
Contributor IV

Hii Yuri ,

I have finished my secure boot work for u boot an now I am going to work with zImage .

Can you please tell me the changes needs to be done in kernel .

Regards ,

Pramod

0 Kudos
Reply
2 Replies

1,196 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Please refer to Appendix G (Extending the root of trust) of app note "Secure Boot on i.MX 50,

i.MX 53, i.MX 6 and i.MX 7 Series using HABv4", Rev. 2, 05/2018.

https://www.nxp.com/docs/en/application-note/AN4581.pdf 


Have a great day,
Yuri

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,196 Views
PramodKumar
Contributor IV

Hii Yuri ,

I have created the zIMage-signed-pad.bin file after merge of csf and ivt file .

Now , I Know that how to load it in mmc from uboot command prompt but , how can we copy the signed_zImage.bin file in sd card ? Is it called by uboot .

Regards ,

Pramod

0 Kudos
Reply