HAB bin to Imx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HAB bin to Imx

2,110件の閲覧回数
aishashaik
Contributor II

1.We used HAB user manual for generating HAB enabled bin.So  how to convert the HAB enabled bin to Imx file.If IVT is required how i can include the IVT to bin to get imx.?

2.Is any other tool available to convert bin file to imx?

3.Any other support files we need to take care during the conversion of bin to imx ?

4.Whether the bin to imx conversion is work out for Android?

ラベル(2)
3 返答(返信)

1,899件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Aisha

it may be useful to look at automatic secure u-boot.imx and zImage generation scripts :

imx-test-3.14.28-1.0.0/.../mxc_secureboot/   folder

http://repository.timesys.com/buildsources/i/imx-test/imx-test-3.14.28-1.0.0/

Workshop - Android  Secure Boot

https://community.freescale.com/docs/DOC-104799

https://community.freescale.com/community/imx/i.mx-training/training-security/training-secure-boot/i...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,899件の閲覧回数
senthilkumar_s1
Contributor II

Dear,

I wasn't able to view the below links that you had shared earlier in the conversation.

https://community.freescale.com/docs/DOC-104799

https://community.freescale.com/community/imx/i.mx-training/training-security/training-secure-boot/i...

It says unauthorized access.Please help us in getting those documents.

Thanks,

Senthil

0 件の賞賛
返信

1,899件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Senthil

please ask for access local fae.

Best regards

igor

0 件の賞賛
返信