HAB Secure Boot and ARM Trusted Firmware

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HAB Secure Boot and ARM Trusted Firmware

ソリューションへジャンプ
4,392件の閲覧回数
nikhil29
Contributor III

Hello NXP TechSupport



I'm working on i.MX 8M Mini EVK Board with LPDDR4

 

1] Do this Mini EVK having support of HAB Secure Boot and ARM Trusted Firmware ??

2] What are the uses of HAB Secure Boot and ARM Trusted Firmware ??

3] is it essential to flash on EVK ??



Thanks
Nikhil

0 件の賞賛
返信
1 解決策
4,371件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nikhil

 

1] Do this Mini EVK having support of HAB Secure Boot and ARM Trusted Firmware ??

 

yes

 

>2] What are the uses of HAB Secure Boot and ARM Trusted Firmware ??

 

secure boot prevents hackers to alter the boot process, short description can be found on

https://boundarydevices.com/high-assurance-boot-hab-dummies/

ATF description

https://community.arm.com/developer/tools-software/oss-platforms/w/docs/483/trusted-firmware-a

 

>3] is it essential to flash on EVK ??

 

no

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
4,372件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nikhil

 

1] Do this Mini EVK having support of HAB Secure Boot and ARM Trusted Firmware ??

 

yes

 

>2] What are the uses of HAB Secure Boot and ARM Trusted Firmware ??

 

secure boot prevents hackers to alter the boot process, short description can be found on

https://boundarydevices.com/high-assurance-boot-hab-dummies/

ATF description

https://community.arm.com/developer/tools-software/oss-platforms/w/docs/483/trusted-firmware-a

 

>3] is it essential to flash on EVK ??

 

no

 

Best regards
igor

0 件の賞賛
返信
3,257件の閲覧回数
mcuboot
Contributor II

Hi,

 

Where is the code for ATF for i.MX8M mini? Can it be found in linux kernel or yocto download?

0 件の賞賛
返信
4,359件の閲覧回数
nikhil29
Contributor III

Thanks igor

 

I understood the entire concept : HAB Secure Boot and ARM Trusted Firmware.

 

Regards

Nikhil

0 件の賞賛
返信