HAB_IMX6UL_STEPS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HAB_IMX6UL_STEPS

3,386 Views
PramodKumar
Contributor IV

Hii Team ,

How to start secure boot in imx6ul ?  My host PC is of 64 bit but my imx machine is of 32 bit , share the steps .

I have installed the openssl with updated version & cst tool 3.1.10 version .

Have a great day  ,

Pramod Kumar

Labels (2)
6 Replies

3,248 Views
igorpadykov
NXP Employee
NXP Employee

Hi Pramod 

one can look at latest uboot documentation

habv4\imx\doc - uboot-imx - i.MX U-Boot 

and secure boot app notes on

i.MX 6Quad Applications Processors | Quad Arm® Cortex®-A9 | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,248 Views
PramodKumar
Contributor IV

Hii ,

Can you please share the exact steps for the same , from scratch on-wards .

0 Kudos
Reply

3,248 Views
PramodKumar
Contributor IV

Hii Igor ,

I need to ask you that what changes we need to done in uboot to make the uimage for secure boot enabled .

Regards

Pramod .

0 Kudos
Reply

3,248 Views
PramodKumar
Contributor IV

What is this command for :

echo -e "o""\n""n""\n""p""\n""1""\n""2048""\n""+256M""\n""w" | sudo fdisk /dev/sdb

0 Kudos
Reply

3,248 Views
PramodKumar
Contributor IV

The documents are too much helpful but I am confused between encryption based codes and secure based codes .

Can you clarify me for that .

0 Kudos
Reply