H263 Encoder

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

H263 Encoder

Jump to solution
2,038 Views
muhammadhumayun
Contributor I

Hi,

I want to user H263 harware encoder available on IMX53 Sabre tablet using android. Stagefright does not include the support  of VPU in the default port of android I get from freescale site. If stagefright does not include the H263 hardware encoder then how i can use in the Saber tablet?

Thanks,

Humayun

Labels (3)
0 Kudos
Reply
1 Solution
1,853 Views
Yongxin
NXP Employee
NXP Employee

Please refer section 3.2.2.7 "EncH263Param" in i.MX5x_Linux_VPU_API.pdf

View solution in original post

0 Kudos
Reply
1 Reply
1,853 Views
Yongxin
NXP Employee
NXP Employee

Please refer section 3.2.2.7 "EncH263Param" in i.MX5x_Linux_VPU_API.pdf

0 Kudos
Reply