H.264 sample video

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

H.264 sample video

跳至解决方案
2,639 次查看
tetsuomaeda
Contributor III

Hi,

This is my first question at this forum.

We are thinking to use iMX6 series for our H.264 video encoding platform.

The target bit rate is 14Mbps at 1920 x 1080p resolution.

1. Are there any sample encoded video that can be used for our evaluation?

2. Is there a software encoder which emulates the quality of the iMX6 H/W encoder?

.

Thanks in advance for the information.

Tetsuo.

标签 (2)
标记 (3)
0 项奖励
回复
1 解答
2,408 次查看
igorpadykov
NXP Employee
NXP Employee

Hi TETSUO

I am afraid there are no such samples or test apps.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,409 次查看
igorpadykov
NXP Employee
NXP Employee

Hi TETSUO

I am afraid there are no such samples or test apps.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,408 次查看
tetsuomaeda
Contributor III

Hi Igor-san,

Thank you for the reply.

I'll look for other method.

Regards,

Tetsuo

0 项奖励
回复