H.264 sample video

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

H.264 sample video

Jump to solution
2,676 Views
tetsuomaeda
Contributor III

Hi,

This is my first question at this forum.

We are thinking to use iMX6 series for our H.264 video encoding platform.

The target bit rate is 14Mbps at 1920 x 1080p resolution.

1. Are there any sample encoded video that can be used for our evaluation?

2. Is there a software encoder which emulates the quality of the iMX6 H/W encoder?

.

Thanks in advance for the information.

Tetsuo.

Labels (2)
Tags (3)
0 Kudos
Reply
1 Solution
2,445 Views
igorpadykov
NXP Employee
NXP Employee

Hi TETSUO

I am afraid there are no such samples or test apps.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,446 Views
igorpadykov
NXP Employee
NXP Employee

Hi TETSUO

I am afraid there are no such samples or test apps.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,445 Views
tetsuomaeda
Contributor III

Hi Igor-san,

Thank you for the reply.

I'll look for other method.

Regards,

Tetsuo

0 Kudos
Reply