Guide on setting up Android build for IMX 6 EVk

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Guide on setting up Android build for IMX 6 EVk

1,200 次查看
lyfsci
Contributor III

Hi Experts,

i have downloaded the Android source file from the freescale site for IMX 6 SL EVK board.

I have the following files in the archives.

core_package_manifest.txt

EULA.txt

SCR-android_code_source.txt

and a folder

code

Now how to build the image for the board ??


Regards,

Lyf

标签 (1)
0 项奖励
回复
1 回复

832 次查看
SergioSolis
NXP Employee
NXP Employee

Please take a look at the android user guide, which you can find in the following link:

i.MX 6SoloLite Evaluation Kit|Freescale

File >> i.MX6 Android L5.0.0_1.0.0 BSP Documentation

It will guide you step by step on how to build and flash android on the board.


Have a great day,
Sergio Solis

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复