Gstreamer not working with imx53 custom board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Gstreamer not working with imx53 custom board

981 Views
prasadroy
Contributor I

I am using the mfw_isink plugin for gstreamer for video streaming.

I have set the local alpha feature as export VSALPHA=1 and launch the gstreamer using below command.

 

gst-launch mfw_v4lsrc  device=/dev/video0  ! mfw_isink

 

I am seeing only colored lines in the display and  not able to stream the video.

The log details are given below.

  

MFW_GST_V4LSRC_PLUGIN 2.0.3 build on Jun 15 2017 10:07:07.

set color key

MFW_GST_ISINK_PLUGIN 2.0.3 build on Jun 15 2017 10:06:49.

Setting pipeline to PAUSED ...

In MVC:mxc_streamoff

 

 In MVC:mxc_streamon

IPU:In csi_enc_enabling_tasks

In csi_enc_setup

Pipeline is live and does not need PREROLL ...

Setting pipeline to PLAYING ...

New clock: GstSystemClock

can not create threadmfw_gst_isink_setcaps:1390

VS0 created. in fmt[I420] win(0,0-mxc_ipu mxc_ipu: Channel already disabled 10

mxc_ipu mxc_ipu: Channel already uninitialized 10

176,144:176x144).

mxc_ipu mxc_ipu: Channel already disabled 10

mxc_ipu mxc_ipu: Channel already uninitialized 10

Labels (4)
0 Kudos
Reply
1 Reply

878 Views
igorpadykov
NXP Employee
NXP Employee

Hi Prasad

what bsp used in the case, mainline may have not necessary

vpu hardware plugins. Please try official codecs

Codecs and other Algorithms (1)
IMX53_11_09_LINUX_MMCODECS
http://www.nxp.com/products/automotive-products/energy-power-management/pmics/power-management-for-i...

and follow p.39,40 attached document.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply