Gstreamer network decoding performance

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Gstreamer network decoding performance

1,793件の閲覧回数
timothybean1
Contributor I

Hello all,

I have just purchased a new Nitrogen6x board for testing. My application is a low latency HD decoder. I am interested if anyone can comment as to the latency of decoding a 720p H.264 video stream from the network (RTSP). I would like to know what the expected latency is out-of-the box for the Freescale Gstreamer elements. I have been digging around and found a min_latency setting for the vpudec element that looks like something I would want to use. Can anyone give me some expectations. I am looking for less than 500 ms end-to-end. Is that feasible without modification to the Gstreamer elements?

Thanks

Tim

ラベル(3)
1 返信

1,538件の閲覧回数
timothybean
Contributor IV

The network streaming is very good. Latency is excellent.