Gstreamer and WebM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Gstreamer and WebM

2,572件の閲覧回数
amassa
Contributor II

Hi,

I'm trying to setup my SABRE-SDP board to stream video from a camera using the WebM format. Has anyone successfully done this before?

Any help is greatly appreciated.


Thanks.

ラベル(5)
0 件の賞賛
返信
3 返答(返信)

2,411件の閲覧回数
amassa
Contributor II

Also, I am using: Linux version 3.10.17-1.0.0_ga+g232293e (jenkins@yocto-buildthree)

0 件の賞賛
返信

2,411件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

could you give me more detailed information? what web camera do you use and what OS do you need ?

0 件の賞賛
返信

2,411件の閲覧回数
amassa
Contributor II

I have both cameras on the SABRE board, but I think the ov5642 is the only one I've been able to get running. I am running a downloaded Yocto release on the SABRE board. I have it connected via ethernet to a Windows PC. I've used the ov5642-mx6qsdp-stream.pdf doc and was able to get that up and running.

I get errors trying to use vp8enc with webm. I'm not sure if that's needed or not.

Thanks.

0 件の賞賛
返信