Green dots and lines in LCD display

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Green dots and lines in LCD display

3,229 Views
yashavanthashet
Contributor V

Hi,

I am using i.MX8M custom board with android Pie9.0 release.
Here some green dots are observed in display. The green lines are observed more when I play video in LCD. I am using Raydium rm67198 display. (attached image of lcd).

The LCD display worked fine with 4.9.51 Linux release with same display driver.


The same issue is not observed when I play video in HDMI.

Thanks in advance.

Best Regards,
Yashavantha

0 Kudos
Reply
4 Replies

3,073 Views
yashavanthashet
Contributor V

Hi,

Regarding above issue, if "disable hw overlays" property is enabled in developer options then the issue will be solved.

Is enabling above property is needed?

Regards,

Yashavantha

0 Kudos
Reply

3,073 Views
joanxie
NXP TechSupport
NXP TechSupport

we don't reproduce this issue on the imx8M evk board, what ddr size you use in your own board? this maybe the gpu hardware limitation issue, I got information that GPU hardware has limitation to access the physical memory address > 0x80000000

0 Kudos
Reply

3,073 Views
yashavanthashet
Contributor V

We are using 2GB DDR in our board.

Regards,

Yashavantha

0 Kudos
Reply

3,073 Views
joanxie
NXP TechSupport
NXP TechSupport

because of gpu limitation, try to change the source code as below:

Kernel: arch/arm/boot/dts/imx6q.dtsi
Modify to following:
linux,cma {
                        compatible = "shared-dma-pool";
                        reusable;
                        alloc-ranges = <0x40000000 0x40000000>;
                        size = <0x40000000>;
                        linux,cma-default;
          };
 It means that CMA address begin from 0x40000000, CMA size is 0x40000000(1GB), 0x40000000 + 0x40000000 = 0x80000000.
Customer can adjust this two values, just make sure that CMA begin and end address < 0x80000000 

0 Kudos
Reply