Good news! Mfgtool source code is released now

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Good news! Mfgtool source code is released now

25,977 Views
StanleyLee
NXP Employee
NXP Employee

Hi there,

 

Mfgtool host tool is uploaded to the forum now. You can revise the tool to add your own functionality, and do debug work by yourself if you meet issues.

 

The tool need below environment to compile:

1. VS2008

2. Windows XP/7 SDK

3. Windows XP/7 WDK

 

For details, please refer to Build_Requirements.docx in mfgtools\Apps\MfgTool.exe\docs

 

And any feedback about the tool is appreciated!

24 Replies

1,361 Views
MarcCoussement
Contributor I

Sorry,

Can't find latest mfgtool source code dowload link.

 

Marc,

0 Kudos
Reply

1,361 Views
x10
Contributor V

Thanks for sharing source code

0 Kudos
Reply

1,361 Views
vishnupatekar
Contributor II
Great!! Thanks for sharing source code.
0 Kudos
Reply

1,361 Views
ChrisWilliamson
Contributor III

AWESOME! Way to go everyone!

Chris

0 Kudos
Reply