Getting flicker in display after starting x11 server (i.MX6)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Getting flicker in display after starting x11 server (i.MX6)

2,230 Views
rizwanm
Contributor II

Hi,

we are using i.MX6 #imx6 dualplus/6quadplus Custom Board.

In that we are observing little flickering once booting up. after pSplash Screen comes,

when starting X11 Server little flickering observed #display flicker‌ x11 #xorg-server

when debugged we have observed various observation,

Below are the Observations.

Ob 1 : while debugging "/etc/init.d/xserver-nodm" in this script file X11 server is starting >>>>>>>> echo "Starting Xserver" >>>>>>>> . /etc/X11/xserver-common >>>>>>>> xinit /etc/X11/Xsession -- `which $XSERVER` $ARGS >/var/log/Xsession.log 2>&1 after commenting above script board boots completely without any flickering but not moving from psplash screen to Yocto desktop after that once enabled, Psplash screen goes then LCD flickers start for 2 - 4 seconds then going to Yocto Linux Home page. #splash_screen

Ob2 : Further debugging in X11 folder under the linux file system we got know one script called "/etc/X11/xorg.conf" in this script #xserver-xorg-video-imx-viv

Section "Device"

      Identifier "i.MX Accelerated Framebuffer Device"

      Driver "vivante"

      Option "fbdev" "/dev/fb0"

      Option "vivante_fbdev" "/dev/fb0"

      Option "HWcursor" "false"

      Option "mode_settings" "false"

EndSection

      Section "ServerFlags"

      Option "BlankTime" "0"

      Option "StandbyTime" "0"

      Option "SuspendTime" "0"

        Option "OffTime" "0"

EndSection

>>>>>> however mode_settings in false but still why X11 starts flickering

Ob 3 : After exploring into in-depth we have got some answered query from

NXP community below are the link,

https://community.nxp.com/thread/328618

in above link same observation has got to one user also they have solved but unfortunately they are using Old Yocto kernel.

We are using Linux 4.1.15 Linux Kernel BSP. #linux kernel 4.1.15#linux bsp#linux-source#linux device tree#freescale bsp

 

0 Kudos
Reply
1 Reply

2,101 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Rizwan,

I am not sure if it is an issue, it is not actually a flicker it is the transition from the splash screen -> terminal -> window manager. I just checked my 5.4.24 bsp on qxp board running xwayland and I see the same behavior, but it is faster.

Regards

0 Kudos
Reply