Getting Ubuntu onto i.MX 8M Mini EVKB evaluation board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Getting Ubuntu onto i.MX 8M Mini EVKB evaluation board

Jump to solution
23,070 Views
rwhitehead
Contributor I

I want to get Ubuntu (18.04 or 20.04)  onto this evaluation board. My target is to run Docker, then I'll build my software in containers.

A colleague has given me instructions for building an image, but so far it has always failed at the bitbake stage with 1 or 2 packages failing to build.

Do I actually need to do that, though? The Quick Start Guide says there are pre-built binaries. I've found the page https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat..., but all the installations listed seem to be "demos".  Is this what I want? 

Should I give up trying to build an image and instead use UUU to "update" the installed Android to an Ubuntu 'demo'?

Sorry to ask what must be a basic question but I find a lot of the documentation unhelpful at my stage of ignorance - I'm sure it helps if you already know what you need to do!.

Labels (2)
0 Kudos
Reply
1 Solution
22,941 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hello rwhitehead

After checking the README.md that you shared and build process. You need to change as below two aspects.

  1. the DISTRO should be imx-desktop-xwayland instead of fsl-imx-xwayland
  2. the image for bitbake should be imx-image-desktop.

Regarding this "do_fetch: Failed to fetch 'runc'", which might be caused by various of ways. As you say that is not a network glitch, for this problem fixed, I would like to recommend you have a try to fix it as followings.

  1. bitbake runc  -c cleansstate  
  2. It would be better to check the directory 'downloads' which is under your bsp directory if there are 'broken' or uncompleted runc files, delete them if any before go next steps.
  3. Manually download and put it under directory 'downloads', meanwhile get a copy of it with suffix extension as .done
  4. bitbake runc -c compile -f
  5. if all goes fine, then bitbake imx-image-desktop

Regarding that pre-built binaries are available

NXP does not release desktop image due to the license.

 

I have attached the release note for your further reference.

 

Best regards

Harvey

View solution in original post

17 Replies
22,366 Views
josephzhou1
Contributor V
branch=master

 

is the problem  due to all branch name now  are changed from master to main ( see 

github.com/

).

 

thanks 

Best Regards,
Joseph Zhou Jianhui / Senior Embedded Software Engineer, Singapore
0 Kudos
Reply
23,034 Views
rwhitehead
Contributor I

Harvey,

I attached my build instructions above. They seem to correspond to your document, but my colleague has already spent many hours fixing issues, as you will see he has added quite a bit of detail and some fixes which were not apparent from your document.

I ask yet again: Is there a pre-built image? I can see some "demo" images, will those act as a linux installation? Can you build these without the demo?

0 Kudos
Reply
22,940 Views
Harvey021
NXP TechSupport
NXP TechSupport

Can you build these without the demo?

Yes, I just successfully build it again according to the steps following up the i.MX_Desktop_Users_Guide

 

Best Regards

Harvey

0 Kudos
Reply
23,040 Views
rwhitehead
Contributor I

Thanks for your help.

I’ve attached my instructions in case you can see anything wrong – they seem to correspond to your document.
I have tried building versions 5.10.52-2.1.0 and 5.10.72-2.2.0.
This is what I get with 5.10.72-2.2.0. It talks about a failure fetch from a repo - note that this has persisted over a week, it is not a network glitch.

I still can't see why I need to build this - NXP claims that "pre-built binaries are available" - where are they?

 

$ bitbake imx-image-core -c populate_sdk
Loading cache: 100% |############################################################################################################################################################################################| Time: 0:00:01
Loaded 4951 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies
NOTE: Multiple providers are available for runtime linux-firmware-bcm4359-pcie (firmware-nxp-wifi, linux-firmware)
Consider defining a PREFERRED_RPROVIDER entry to match linux-firmware-bcm4359-pcie

Build Configuration:
BB_VERSION           = "1.50.0"
BUILD_SYS            = "x86_64-linux"
NATIVELSBSTRING      = "ubuntu-20.04"
TARGET_SYS           = "aarch64-poky-linux"
MACHINE              = "imx8mmevk"
DISTRO               = "fsl-imx-xwayland"
DISTRO_VERSION       = "5.10-hardknott"
TUNE_FEATURES        = "aarch64 armv8a crc cortexa53 crypto"
TARGET_FPU           = ""
meta                 
meta-poky            = "HEAD:269265c00091fa65f93de6cad32bf24f1e7f72a3"
meta-oe              
meta-multimedia      
meta-python          = "HEAD:f44e1a2b575826e88b8cb2725e54a7c5d29cf94a"
meta-freescale       = "HEAD:469d6c958c76ea235b3d3c1527e797ce3a7392e3"
meta-freescale-3rdparty = "HEAD:f8150f3b37cb83cba1f9e2378e57bb63e02d4610"
meta-freescale-distro = "HEAD:e6daa26ba1f748326546063d63a085ae671827d9"
meta-bsp             
meta-sdk             
meta-ml              
meta-v2x             = "HEAD:320638350cb4c4cc8e7a2db49d5eae0d8a0bdc01"
meta-nxp-demo-experience = "HEAD:9dcc11ea9f525cffedbb28895e0abb443e56c3e0"
meta-chromium        = "HEAD:8be1d3a0ba0cf32e61144900597207af5698c10d"
meta-clang           = "HEAD:b0d805060791006d651efd3d7ae3dd5add8f70fe"
meta-gnome           
meta-networking      
meta-filesystems     = "HEAD:f44e1a2b575826e88b8cb2725e54a7c5d29cf94a"
meta-qt5             = "HEAD:43f8f539d40070a70fe89136db89bf5bb1dfe7ed"
meta-python2         = "HEAD:8db9e4f6ceae33d7a4f55453d31e69f9858af4eb"
meta-virtualization  = "HEAD:7f719ef40896b6c78893add8485fda995b00d51d"

Initialising tasks: 100% |#######################################################################################################################################################################################| Time: 0:00:08
Sstate summary: Wanted 1389 Local 0 Network 0 Missed 1389 Current 1050 (0% match, 43% complete)
NOTE: Executing Tasks
WARNING: runc-opencontainers-1.0.0-rc93+gitAUTOINC+249bca0a13-r0 do_fetch: Failed to fetch URL git://github.com/opencontainers/runc;branch=master, attempting MIRRORS if available
ERROR: runc-opencontainers-1.0.0-rc93+gitAUTOINC+249bca0a13-r0 do_fetch: Fetcher failure: Unable to find revision 249bca0a1316129dcd5bd38b5d75572274181cb5 in branch master even from upstream
ERROR: runc-opencontainers-1.0.0-rc93+gitAUTOINC+249bca0a13-r0 do_fetch: Fetcher failure for URL: 'git://github.com/opencontainers/runc;branch=master'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/richard/Zebra/projects/Edge_AI/performance/rnw-performance-measure/imx8-build/imx-yocto-bsp/build/tmp/work/cortexa53-crypto-poky-linux/runc-opencontainers/1.0.0-rc93+gitAUTOINC+249bca0a13-r0/temp/log.do_fetch.825
ERROR: Task (/home/richard/Zebra/projects/Edge_AI/performance/rnw-performance-measure/imx8-build/imx-yocto-bsp/sources/meta-virtualization/recipes-containers/runc/runc-opencontainers_git.bb:do_fetch) failed with exit code '1'
NOTE: Tasks Summary: Attempted 4061 tasks of which 4042 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
  /home/richard/Zebra/projects/Edge_AI/performance/rnw-performance-measure/imx8-build/imx-yocto-bsp/sources/meta-virtualization/recipes-containers/runc/runc-opencontainers_git.bb:do_fetch
Summary: There was 1 WARNING message shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

 

 

0 Kudos
Reply
22,942 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hello rwhitehead

After checking the README.md that you shared and build process. You need to change as below two aspects.

  1. the DISTRO should be imx-desktop-xwayland instead of fsl-imx-xwayland
  2. the image for bitbake should be imx-image-desktop.

Regarding this "do_fetch: Failed to fetch 'runc'", which might be caused by various of ways. As you say that is not a network glitch, for this problem fixed, I would like to recommend you have a try to fix it as followings.

  1. bitbake runc  -c cleansstate  
  2. It would be better to check the directory 'downloads' which is under your bsp directory if there are 'broken' or uncompleted runc files, delete them if any before go next steps.
  3. Manually download and put it under directory 'downloads', meanwhile get a copy of it with suffix extension as .done
  4. bitbake runc -c compile -f
  5. if all goes fine, then bitbake imx-image-desktop

Regarding that pre-built binaries are available

NXP does not release desktop image due to the license.

 

I have attached the release note for your further reference.

 

Best regards

Harvey

22,905 Views
rwhitehead
Contributor I

Harvey,

It built! Thank you very much for your help.

Please can you explain what to do next? The Desktop Users Guide says "Building imx-boot and UUU:
The build method is the same as the i.MX Yocto Project", and refers to the Linux Users Guide, which has many options that I don't understand. It seems to hint that putting the image on SD card would be easiest (section 4.3) but I don't understand where to start. Have I now built the iamge or do I need to run bitbake again and make the SDK (I don't understand what the SDK is)?

Thanks again.

Richard

0 Kudos
Reply
22,860 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hello rwhitehead.

Regarding UUU: please refer to the link where you will see details about it.

Release 1.4.193 · NXPmicro/mfgtools · GitHub

Regarding SDK: please refer to the link: Welcome | MCUXpresso SDK Builder (nxp.com)

Regarding that "It seems to hint that putting the image on SD card would be easiest (section 4.3)"

You can use Tool uuu or dd to load the image that you desire to SD card which then can be inserted into target(assume i.MX8MM) to start. for image, as this case, it will be the one that you build it.

 

Best regards

Harvey.

 

0 Kudos
Reply
22,929 Views
rwhitehead
Contributor I

Harvey,

That’s great, thank you.

I don’t actually need a desktop install, I am happy to work with it over SSH and would like as much room on the device as possible. My colleague built the “core” build for this same reason.

Please can you tell me the name of the “core” image in the imx-desktop-xwayland distro?

Also, since I don’t need the desktop, is there a pre-built image of the core linux?

I am very confused by all the different suggestions now; I am going to try a clean build following this latest suggestion from you.

Thanks very much,

Richard

0 Kudos
Reply
22,879 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hello rwhitehead.

For Ubuntu build, it just provides the build for imx-image-desktop.

For pre-built image of the core linux, due to the release license limit, so no pre-built image, please check with the release note that I shared last time.

 

Best Regards

Harvey

0 Kudos
Reply
22,864 Views
rwhitehead
Contributor I

Harvey,

Replies seem to be getting out of order in the message board and you have replied to something I asked a few days ago. You already explained so sorry about the confusion.

I have built the image now following your instructions, thank you so much. I compared my colleague's instructions to yours and could not see the difference, which you spotted, so well done and much appreciated.

The last question I asked was:

Please can you explain what to do next? The Desktop Users Guide says "Building imx-boot and UUU:
The build method is the same as the i.MX Yocto Project", and refers to the Linux Users Guide, which has many options that I don't understand. It seems to hint that putting the image on SD card would be easiest (section 4.3) but I don't understand where to start. Have I now built the iamge or do I need to run bitbake again and make the SDK (I don't understand what the SDK is)?

Thanks again.

Richard

0 Kudos
Reply
22,920 Views
josephzhou1
Contributor V

1

hi there, great! you are on the right track.

2

super correct! i am also strongly to support u just only redo a fully sync repo and bitbake , simply get  correct your build , not need go too far too complicate and too confuse way lah

 

3

please update here u settled it or not , good lucky!

thank you

 

PS:

  1. bitbake runc  -c cleansstate  
  2. bitbake runc -c compile -f
  3. bitbake imx-image-desktop

just as same as  redo, it is clear "status" and goto remote repos to sync (it is the 1), and a fresh compile it lah(it is the 2). and   it is not a tarball .tar.gz manually download the whole Runc?  how can ?! not easy way lah ,heehee. not do this just go to do a fresh build please , thank you 

Best Regards,
Joseph Zhou Jianhui / Senior Embedded Software Engineer, Singapore
0 Kudos
Reply
23,018 Views
josephzhou1
Contributor V
branch=master

 

is the problem  due to all branch name now  are changed from master to main in github , see below you can go yours checkout branch to check it is already " main" branch  not "master":

https://github.com/opencontainers/runc/commit/249bca0a1316129dcd5bd38b5d75572274181cb5

so your layer also must be "main " not "master"

 

also see the meta-virtualization commit c5f61e5  below the new bb is ok already  if you sync yours repos:

 

josephzhou1_0-1644633079343.jpeg

 

solution 1 :

goto :

/home/richard/Zebra/projects/Edge_AI/performance/rnw-performance-measure/imx8-build/imx-yocto-bsp/sources/meta-virtualization/recipes-containers/runc/runc-opencontainers_git.bb

modify " branch = master " to " branch = main" 

 

solution 2: redo all steps to make sure sync latest repo

repo sync 

the latest "meta-virtualization/runc"   shld be ok alry sync to " main " not "master"

(15 days ago, Commits only on Jan 28, 2022,  after that update then it shlb be ok)

 

 

pls try n let m know if ok pls put mine as a soluton pls

 

 

thanks all

Best Regards,
Joseph Zhou Jianhui / Senior Embedded Software Engineer, Singapore
0 Kudos
Reply
23,039 Views
khang_letruong
Senior Contributor III

Hi @rwhitehead,

Bitbake command seems to be wrong, it should be

$ bitbake imx-image-desktop

 for bitbaking Ubuntu based desktop image.

Also, please make sure that the yocto settings prior that step are correct. Instructions are found in iMX_Desktop_User_Guide.pdf in the compressed file attached by @Harvey021 .

 

Regards,
K.

Regards,
k.

0 Kudos
Reply
23,036 Views
rwhitehead
Contributor I

bitbake imx-image-desktop -c populate_sdk
Loading cache: 100% |############################################################################################################################################################################################| Time: 0:00:01
Loaded 4951 entries from dependency cache.
ERROR: Nothing PROVIDES 'imx-image-desktop'. Close matches:
imx-image-core

Summary: There was 1 ERROR message shown, returning a non-zero exit code.

0 Kudos
Reply
23,032 Views
khang_letruong
Senior Contributor III

Hi @rwhitehead ,

Please follow exactly these instructions (2.1 to 2.5) from scratch:

Screenshot from 2022-02-11 19-05-11.png

And DO NOT populate the SDK (remove the -c populate_sdk from the command)

Regards,
K.

0 Kudos
Reply
23,047 Views
khang_letruong
Senior Contributor III
0 Kudos
Reply
23,053 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hello rwhitehead.

I am not sure what the instructions for building an image you have got. Here is a link (https://www.nxp.com/webapp/Download?colCode=i.MX_Desktop_POC_GA_Docs) that might be different one that can be helpful for you, and I also share with you the compressed one as attached for your convenience.

Furthermore, could you please share the error message for those packages failing to build? for purpose that we can investigate into what problems with it.

 

Best regards

Harvey