Getting HAB to auth signed kernel on a MX8Mini

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Getting HAB to auth signed kernel on a MX8Mini

ソリューションへジャンプ
2,690件の閲覧回数
adam_m
Contributor II

I am working on getting uboot to load a secure kernel on a Boundary Devices Nitrogen8MM. I have already worked through the instructions at https://boundarydevices.com/high-assurance-boot-hab-i-mx8m-edition/ and eveything is working with a sigend uboot.

According to BoundaryDevices, they have been told by NXP that the next step is to get booti to auth the kernel by using this patch: https://github.com/boundarydevices/u-boot-imx6/commit/a20a5ee3c0 However, it's not working.

When I auth the kernel by hand using hab_auth_img, it appears to work just fine:

=> load mmc 1 ${loadaddr} Image
30009696 bytes read in 679 ms (42.1 MiB/s)
=> hab_auth_img ${loadaddr} ${filesize} 0x01c9d000

Authenticate image from DDR location 0x40480000...

Secure boot enabled

HAB Configuration: 0xcc, HAB State: 0x99
No HAB Events Found!

=>


But when just booting I get this:

Authenticating Image...

Authenticate image from DDR location 0x40800000...
Error: Invalid IVT structure

Allowed IVT structure:
IVT HDR = 0x4X2000D1
IVT ENTRY = 0xXXXXXXXX
IVT RSV1 = 0x0
IVT DCD = 0x0
IVT BOOT_DATA = 0xXXXXXXXX
IVT SELF = 0xXXXXXXXX
IVT CSF = 0xXXXXXXXX
IVT RSV2 = 0x0
Authenticate Image Fail, Please check
Error loading kernel image


And, of course, if I don't use the patch then it boots just fine, but I need to auth the kernel before leading.

What am I missing?

ラベル(3)
0 件の賞賛
返信
1 解決策
2,641件の閲覧回数
Yuri
NXP Employee
NXP Employee

@adam_m 
Hello,

  Have You used recommendations in U-boot help how to sign kernel?

https://source.codeaurora.org/external/imx/uboot-imx/tree/doc/imx/habv4/guides/mx8m_mx8mm_secure_boo...

 

Regards,
Yuri.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,672件の閲覧回数
adam_m
Contributor II

I've done some digging and the issue seems to be that IVT_SEFT and IVT_INITAL don't match in validate_ivt(). I added some debuggin statements and found this:

Allowed IVT structure:
IVT HDR = 0x4X2000D1
IVT ENTRY = 0xXXXXXXXX
IVT RSV1 = 0x0
IVT DCD = 0x0
IVT BOOT_DATA = 0xXXXXXXXX
IVT SELF = 0xXXXXXXXX
IVT CSF = 0xXXXXXXXX
IVT RSV2 = 0x0
Found values:
IVT_ENTRY: 0x40480000
IVT_RSV1: 0x0
IVT_DCD: 0x0
IVT_SELF: 0x4211d000
IVT_INITAL: 0x4249d000
IVT_CSF: 0x4211d020
IVT_RSV2: 0x0

So, they are off by 0x380000 which is a suspiciously round number, but I can't figure out where it comes from.

0 件の賞賛
返信
2,642件の閲覧回数
Yuri
NXP Employee
NXP Employee

@adam_m 
Hello,

  Have You used recommendations in U-boot help how to sign kernel?

https://source.codeaurora.org/external/imx/uboot-imx/tree/doc/imx/habv4/guides/mx8m_mx8mm_secure_boo...

 

Regards,
Yuri.

0 件の賞賛
返信