Get test image

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Get test image

2,524件の閲覧回数
michael_irsfeld
Contributor I

Hello Community,

I'm very new to that thematic and I hope that you can give me some hints.

For an application I designed a PCB that can interface a camera. The camera sends bayer12, so i my IPU can only save the data without any converting. I use the parallel 16-bit-Port.

For the first step i only want to know if my hardware is designed in a right way, so I want to see a picture.  I think the data in memory represents a black-white-picture, doesn't it?
What do I have to do to get such a picture in a format like bitmap or png?

Thanks for Help!
Michael

ラベル(4)
0 件の賞賛
返信
1 返信

2,411件の閲覧回数
art
NXP Employee
NXP Employee

Q. I think the data in memory represents a black-white-picture, doesn't it?

A. Typically, the Bayer format contains the grayscale data.

Q. What do I have to do to get such a picture in a format like bitmap or png?

A. There is no ready to use solution to convert the captured CSI frame to a file. Try to set up a camera preview via gstreamer software as described in the Chapter 7 "Multimedia" of the attached document.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信