Generic purpose ADC iMX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Generic purpose ADC iMX6

跳至解决方案
15,573 次查看
caiopereira
Contributor III

I would like to use the ADC to monitoring an analog signal in my board.

A very basic question.

How to use the ADC in iMX6?

How could I setup the adc in the device tree? Could I use the fsl,imx25-adc  driver on imx6 ?

Thank you very much

Best Regards,

Caio Pereira

标签 (2)
1 解答
12,926 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Caio

only i.MX66SX,UL have ADC, test procedure can be found in

attached Linux Manual Chapter 56 ADC Driver

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
12,927 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Caio

only i.MX66SX,UL have ADC, test procedure can be found in

attached Linux Manual Chapter 56 ADC Driver

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

12,926 次查看
caiopereira
Contributor III

Thank you igorpadykov

0 项奖励
回复