Generating a clock on SSP2_SCK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Generating a clock on SSP2_SCK

1,531 Views
danbocko
Contributor I

I have been trying to configure an i.MX287 to generate a clock on SSP2_SCK with no success. I used the OBDS as a starting point. I have also been reading Section 10 of the i.MX28 Applications Processor Reference Manual, this is from section 10.2.3;

"This clock gating is instantiated using an ICG element from the standard cell library."

What is an ICG element and how do I use it? An Internet search provided no useful information. 

Thanks

Dan

Labels (1)
0 Kudos
Reply
1 Reply

1,448 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dan

on i.MX28 EVK this signal is used for spi-nor and one can look at patches on

How to enable SPI NOR boot for i.MX28 (Spansion s25fl256s) 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply