GenAVB/TSN Milan examples

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

GenAVB/TSN Milan examples

2,353 次查看
caconeta1234
Contributor I

Hi there,

I'm trying to use the GenAVB/TSN stack.

Looking at the PROFILEs provided, there aren't many Milan profiles and more specifically, the Milan examples are very limited. Can anyone confirm that 96 KHz 2/4 channels streaming is possible for Milan?

Thank you.

标记 (2)
0 项奖励
回复
3 回复数

1,095 次查看
Niko9
NXP Employee
NXP Employee

can the GenAVB/TSN MiLAN be used in ARM M7?

0 项奖励
回复

2,320 次查看
caconeta1234
Contributor I

Thanks! Unfortunately the quoted text seemed to be mentioned only for a specific PROFILE, so it's not clear that it's a platform problem.

Do you know if that's a limitation of current GenAVB implementation or it's those specific EVKs that would not work? Would it also hold for an IMX8MM based platform even if it has the correct media clock recovery hardware patches?

Thanks.

0 项奖励
回复

2,325 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes milan is supported just the MX6ULL and MX8MP can not support 96KHz and above.

https://www.nxp.com/docs/en/user-guide/GENAVBTSNUG.pdf

 

Regards

0 项奖励
回复