GenAVB/TSN Milan examples

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GenAVB/TSN Milan examples

2,363件の閲覧回数
caconeta1234
Contributor I

Hi there,

I'm trying to use the GenAVB/TSN stack.

Looking at the PROFILEs provided, there aren't many Milan profiles and more specifically, the Milan examples are very limited. Can anyone confirm that 96 KHz 2/4 channels streaming is possible for Milan?

Thank you.

タグ(2)
0 件の賞賛
返信
3 返答(返信)

1,105件の閲覧回数
Niko9
NXP Employee
NXP Employee

can the GenAVB/TSN MiLAN be used in ARM M7?

0 件の賞賛
返信

2,330件の閲覧回数
caconeta1234
Contributor I

Thanks! Unfortunately the quoted text seemed to be mentioned only for a specific PROFILE, so it's not clear that it's a platform problem.

Do you know if that's a limitation of current GenAVB implementation or it's those specific EVKs that would not work? Would it also hold for an IMX8MM based platform even if it has the correct media clock recovery hardware patches?

Thanks.

0 件の賞賛
返信

2,335件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes milan is supported just the MX6ULL and MX8MP can not support 96KHz and above.

https://www.nxp.com/docs/en/user-guide/GENAVBTSNUG.pdf

 

Regards

0 件の賞賛
返信