Galcore module initialization failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Galcore module initialization failed

1,786 Views
massi_
Contributor I

Hello,

we are trying to set up our environment for i.mx6dl bsp, based on Yocto Sumo. We have tried both Linux Kernel 4.9.67 and 4.9.88, but we have several problems in Galcore module initialization. Galcore module (version 6.2.4) is loaded into the Kernel but it is not correctly initialized.

During the Kernel startup, the following log is shown:
"galcore: loading out-of-tree module taints kernel"

Anyway, this procedure is not able to create a device entry as "/dev/galcore".
Could you please provide me a way to fix this issue?

Thanks.

0 Kudos
Reply
1 Reply

1,712 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Massimo,

If you playing with 4.9.88 the galcore is enable by default, in the 4.9.67 the galcore don´t support this kernel, also i suggest to try the 4.14.88 where a lot of bugs fixed

Regards

0 Kudos
Reply