Galcore does not create a device

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Galcore does not create a device

跳至解决方案
3,169 次查看
MicMoba
Contributor V

Hi,

I need some support around the GPU topic of the iMX8MP.

After I switched from Kernel 5.15.52 to Kernel 6.6.23 my LVDS display did not work as expect.

I recognized that the galcore kernel module did not create a device (/dev/galcore).

How can I found out why the device is not create? I tried to remove the module and insert again but this works without error messages. I searched in dmesg and journalctl but also with no success.

 

So what possibilities do I have to get more information? 

标记 (4)
0 项奖励
回复
1 解答
3,033 次查看
MicMoba
Contributor V

Hi I found out that I miss to enable the mix_gpu_ml node in the devicetree.

After I add the lines

&mix_gpu_ml {
	status = "okay";
};

and reboot I have a /dev/galcore device. And now I am also able to start weston

在原帖中查看解决方案

8 回复数
3,075 次查看
MicMoba
Contributor V

I checked the following things:

$ strings /usr/lib/libGAL.so | grep VERSION
  $VERSION$6.4.11:745085:bc7b6a2a0f$

$ strings /usr/lib/modules/6.6.23-v6.6.23-2.0.0-phy-ge2011246/updates/galcore.ko | grep VERSION
  $VERSION$6.4.11:745085$

$ldconfig -p | grep libGAL.so
  libGAL.so (libc6,AArch64) => /lib/libGAL.so

So the Galcore firmware (libGAL.so) and the kernel module (galcore.ko) have the same version. I can see the galcore with lsmod command.

I have a /dev/dri/card0 device but no /dev/galcore device

Which possibilities do I have to do further checks? How is the connection between LVDS and Galcore?

 

0 项奖励
回复
3,067 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You have galcore in your system and it's ready to use, you just need to send the graphics to lvds, make sure your display is lvds in uboot.

Regards

0 项奖励
回复
3,059 次查看
MicMoba
Contributor V

That's a point I will check.

You mean it is not necessary to have a device called /dev/galcore ? I thought this is mantandory for a iMX8 system with Vivante GPU.

This is a part of weston 12 output:

 

 

[12:26:48.568] libseat: session control granted
[12:26:48.571] using /dev/dri/card0
[12:26:48.571] DRM: supports atomic modesetting
[12:26:48.571] DRM: does not support GBM modifiers
[12:26:48.571] DRM: does not support async page flipping
[12:26:48.571] DRM: supports picture aspect ratio
[12:26:48.571] Loading module '/usr/lib/libweston-12/gl-renderer.so'
[     1] Failed to open device: No such file or directory, Try again...
[     2] Failed to open device: No such file or directory, Try again...
[     3] Failed to open device: No such file or directory, Try again...
[     4] Failed to open device: No such file or directory, Try again...
[     5] _OpenDevice(1031): FATAL: Failed to open device, errno=No such file or directory.
[     6] Failed to open device: No such file or directory, Try again...
[     7] Failed to open device: No such file or directory, Try again...
[     8] Failed to open device: No such file or directory, Try again...
[     9] Failed to open device: No such file or directory, Try again...
[    10] _OpenDevice(1031): FATAL: Failed to open device, errno=No such file or directory.
[12:26:56.585] [seatd/client.c:471] Client disconnected

 

 

I thought the "Failed to open device" messages were from a missing /dev/galcore device. How can I get more information about the missing file or directory?

标记 (2)
0 项奖励
回复
3,034 次查看
MicMoba
Contributor V

Hi I found out that I miss to enable the mix_gpu_ml node in the devicetree.

After I add the lines

&mix_gpu_ml {
	status = "okay";
};

and reboot I have a /dev/galcore device. And now I am also able to start weston

3,088 次查看
mgordon
Contributor I

I'm seeing the same issue with 5.4. galcore driver is loaded, but no /dev/galcore device.  Nothing in either dmesg or journalctl. Any suggestions?

 

0 项奖励
回复
3,139 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Send us you dmesg log file is not possible not building the galcore in 6.6.23.

regards

 

0 项奖励
回复
3,104 次查看
MicMoba
Contributor V

Can you tell me how the procedure with the vivante galcore firmare is?

The firmware is a binary blob. The kernel module loads the firmware and initialize the GPU. Is the firmware part of the kernel module (galcore.ko) or should there a .bin file in the /lib/firmware folder which is load?

0 项奖励
回复
3,136 次查看
MicMoba
Contributor V

Hi,

you will find the dmesg output in the attachment

0 项奖励
回复