GUI does not start when enabling GPU profiling from kernel command line

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GUI does not start when enabling GPU profiling from kernel command line

1,837 Views
oussama
Contributor III

I'm using kernel 3.10.17 with yocto rootfs. The kernel is built with CONFIG_MXC_GPU_VIV=y.

When I add "gpuProfiler=1" to the kernel command line, then the yocto qt GUI won't start.

Do I miss something?

Tags (3)
0 Kudos
Reply
1 Reply

1,691 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi oussama,

Vprofiler does not work properly on 3.10.17 and X11 - QT yocto backends, you should try the 3.10.53 kernel base that includes the 5.0.11p1 Vivante driver.

Have a great day,
Alfredo

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply