GUI Image with buildroot for IMX8MM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GUI Image with buildroot for IMX8MM

ソリューションへジャンプ
3,853件の閲覧回数
kanakshilledar
Contributor II

Hi,

I am trying to develop a GUI image for IMX8MM using buildroot. 

Are there any reference defconfigs for such example? If not what are the major packages to be selected while building? I want to build on wayland.

 

Thanks!

0 件の賞賛
返信
1 解決策
3,694件の閲覧回数
gary_bisson
Senior Contributor III

Hi,

You can use the configuration below meant for Ezurio devices:

https://github.com/boundarydevices/buildroot-external-boundary/blob/master/configs/nitrogen8mm_qt5_g...

It includes weston & qt.

Regards

元の投稿で解決策を見る

8 返答(返信)
3,823件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @kanakshilledar 

I hope you are doing very well.

 

Unfortunately there are not buildroot examples. At this moment we just provide support to Yocto.

 

Best regards,

Salas.

0 件の賞賛
返信
3,808件の閲覧回数
kanakshilledar
Contributor II

Hello @Manuel_Salas 

I’m doing well—hope you are too!

Unfortunately there are not buildroot examples.

Thank you for the clarification. Since there are no official Buildroot examples, I wanted to ask: I noticed there are some i.MX8MM-related defconfigs in the Buildroot tree. Are these community-maintained, or contributed by NXP at some point?

Best Regards

 

0 件の賞賛
返信
3,784件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @kanakshilledar 

Could you please share the links or examples of defconfig for buildroot?

Then, I can share information if those are community contributed.

 

Best regards,

Salas.

0 件の賞賛
返信
3,740件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @kanakshilledar 

 

Yes, those repos are external and are not supported by NXP. But it is interesting there are a lot of the NXP devices, maybe I can try one of them and test by my side at the end of the week. 

 

Also, you can try to compile for your desired device and check if those are working or not.

 

Best regards,

Salas.

0 件の賞賛
返信
3,719件の閲覧回数
kanakshilledar
Contributor II

Hello @Manuel_Salas 

These configs are working, but all of them are without GUI, I am looking at ones with GUI.

 

Thanks!

0 件の賞賛
返信
3,695件の閲覧回数
gary_bisson
Senior Contributor III

Hi,

You can use the configuration below meant for Ezurio devices:

https://github.com/boundarydevices/buildroot-external-boundary/blob/master/configs/nitrogen8mm_qt5_g...

It includes weston & qt.

Regards

3,676件の閲覧回数
kanakshilledar
Contributor II

Hi @gary_bisson 

Thanks for sharing those. I will go through it.

 

Best Regards,

0 件の賞賛
返信