GStreamer gst-launch faces latency issues.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GStreamer gst-launch faces latency issues.

2,962件の閲覧回数
donjacobvellathottam
Contributor III

I'm using an i.MX 8 board. I have tried to play a video file using gst-play-1.0, but the video playback is getting stuck at various points. below is the warning message shown:

Redistribute latency...
Redistribute latency...
Redistribute latency...     
WARNING A lot of buffers are being dropped.
WARNING debug information: ../git/libs/gst/base/gstbasesink.c(3143): gst_base_sink_is_too_late (): /GstPlayBin:playbin/GstPlaySink:playsink/GstBin:vbin/GstWaylandSink:waylandsink0:

 

I'm using yocto builds to run the board. The issue with GStreamer is only faced in linux 5.15 and it works perfectly in linux 5.4 

But I need to implement it in 5.15 what may be the reason to this

0 件の賞賛
返信
1 返信

2,938件の閲覧回数
donjacobvellathottam
Contributor III

I'm just posting this here because I think it will be helpful to someone.
So, the issue was with the pipeline. When I changed the pipeline, the issue has been solved.

The pipeline which worked is 

gst-launch-1.0 filesrc location=<filename.mp4> ! qtdemux name=d d.video_0 ! queue ! h264parse ! v4l2h264dec ! imxvideoconvert_g2d ! queue ! waylandsink

0 件の賞賛
返信