GST-Inspect causes kernel paging error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GST-Inspect causes kernel paging error

2,762 Views
chintanchoksi
Contributor I

Hi,

I want to playback audio file from my board. I have installed GStreamer for that on my I.MX35 based custom board. I have Timesys linux installed on my board.

I have installed following G-Streamer packages on my board.

GStreamer-0.10.36

gst-ffmpeg

gst-fsl-plugin

gst-plugins-bad

gst-plugins-base

gst-plugins-farsight

gst-plugins-good

gst-plugins-ugly

fsl-mm-aacpdec-codeclib

fsl-mm-codeclib

When I do gst-inspect on my board, It has kernel paging error. and it does not list all the "mfw" plug-ins.

Can Anyone help me with this ? I have attached the logs for the reference.

Original Attachment has been moved to: Error_Logs_Upload.txt.zip

Labels (1)
0 Kudos
Reply
4 Replies

2,600 Views
Yuri
NXP Employee
NXP Employee

Hello,

  You may try to adapt the following package :

https://www.nxp.com/webapp/Download?colCode=IMX35_25_0912_LINUX_MMDOC_BUNDLE&location=null

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,600 Views
chintanchoksi
Contributor I

Sorry for late reply

I am using Timesys Linux package with my Imx35 board. It has following packages.

gstreamer-0.10.36

gst-plugins-good-0.10.31

gst-plugins-base-0.10.36

gst-fsl-plugin-1.9.5

fsl-mm-codeclib-1.9.5

imx-lib-10.12.01

I have integrated following packages as mentioed in document shared in eariler post. Still I see kernel paging error.

gstreamer-0.10.25

gst-plugins-good-0.10.16

gst-plugins-base-0.10.25

gst-fsl-plugin-1.7.1

fsl-mm-codeclib-1.7.1

imx-lib-09.12.01

Can anyone help me regarding this ???

0 Kudos
Reply

2,600 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello

0 Kudos
Reply

2,600 Views
chintanchoksi
Contributor I

Hi,

I am developing my application using gstreamer. Getting Gstreamer work is my first priority. Alsa drivers are good. I have already tried that.

0 Kudos
Reply