GPU2D failed in i.MX8M

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

GPU2D failed in i.MX8M

跳至解决方案
3,652 次查看
balasubramaniyam
Contributor II

Hi,

I am using the yocto Morty release and Linux 4.9.51 kernel "Linux prebuilt binaries" from NXP website for i.MX8 MQEVK board.

While running "gputop" it show only GPU3D core and GPU2D/VG core remains 0

OUTPUT:

Clients attached to GPU | 0 / 6 (sample_mode: TIME - 1.0 secs)
Galcore version:6.2.4.150331, gpuperfcnt:c122d9db0de3, 1.4
HW:3D:GC7000,Rev:6214
3D Cores:1,2D Cores:0,VG Cores:0

DDR0: r:300.51,w:0.16
DDR1:

PID RES(kB) CONT(kB) VIRT(kB) Non-PGD(kB) Total(kB) CMD
3193 33810 0 0 0 33810 weston
3202 24216 0 0 0 24216 weston-desktop-
3201 3980 0 0 0 3980 weston-keyboard

TOT: 62006 0 0 0 62006
TOT_CON: - - - - 69065

And got the GPU2D clk_get fail message from "dmesg"

[ 5.445259] galcore: loading out-of-tree module taints kernel.
[ 5.459561] galcore: clk_get 2d core clock failed, disable 2d/vg!
[ 5.465762] Galcore version 6.2.4.150331

GPUINFO:

root@imx8mqevk:~# cat /sys/kernel/debug/gc/info
gpu      : 0
model    : 7000
revision : 6214
product  : 70002
eco      :    0

root@imx8mqevk:~# cat /sys/kernel/debug/gc/meminfo

VIDEO MEMORY:
    gcvPOOL_SYSTEM:
        Free  :   70721048 B
        Used  :   63496680 B
        MinFree  :   63654192 B
        MaxUsed  :   70563536 B
        Total :  134217728 B
    gcvPOOL_CONTIGUOUS:
        Used  :          0 B
    gcvPOOL_VIRTUAL:
        Used  :          0 B

NON PAGED MEMORY:
    Used  :          0 B

 

Is i.MX8QM supports GPU2D/VG?

Best Regards,

Bala

0 项奖励
回复
1 解答
2,672 次查看
gary_bisson
Senior Contributor III

Hi,

Please make sure to look at the i.MX8M product page:

i.MX 8M Applications Processor | Arm® Cortex®-A53, Cortex-M4 | 4K display resolution |NXP 

You'll see i.MX8M doesn't have a 2G GPU ;-)

Regards,

Gary

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,672 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Thats correct!

0 项奖励
回复
2,673 次查看
gary_bisson
Senior Contributor III

Hi,

Please make sure to look at the i.MX8M product page:

i.MX 8M Applications Processor | Arm® Cortex®-A53, Cortex-M4 | 4K display resolution |NXP 

You'll see i.MX8M doesn't have a 2G GPU ;-)

Regards,

Gary

0 项奖励
回复