GPU driver not loading in Windows IoT LTSC 2021 image with i.MX8M Plus EVK board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPU driver not loading in Windows IoT LTSC 2021 image with i.MX8M Plus EVK board

9,483件の閲覧回数
benlaj1
Contributor I

Hello,

I've been following the i.MX Windows 10 IoT User’s Guide Rev. W1.1.0, 6/2022 to deploy Windows IoT LTSC 2021 image to my i.MX8M Plus EVK board and I was able to successfully install it on board eMMC. I've used the available prebuilt W21H2-1-1-0 binaries injected into Windows IoT LTSC 2021 image and deployed it but I noticed the GPU driver is not loading. 

I've investigated a little and first notice that no display adapter device was reported in device manager. I was surprised since installation procedure injected available drivers from the prebuilt binaries package. I then manually installed the Galcore driver available in the IoTenTonNXP\driver\galcore folder. Unfortunately, driver is not getting loaded and reports the following error:

This device is not working properly because Windows cannot load the drivers required for this device. (Code 31)

{Not Enough Quota}
Not enough virtual memory or paging file quota is available to complete the specified operation.

I also checked setupapi.dev log file and saw this extra detailed error when installing driver:

Device not started: Device has problem: 0x1f (CM_PROB_FAILED_ADD), problem status: 0xc0000017.

Quick internet search are not pointing to tangible solution where I see tweaking page file or virtual memory to slove issue but I'm using clean image with nothing installed or running.

I would really appreciate your support on this in order to see display adapter working and have GPU support.

Regards

0 件の賞賛
返信
16 返答(返信)

9,344件の閲覧回数
jgrijalba
Contributor I

Hi Benla,

did you try out the latest release W1.2.0 from 9/2022 ?

Regards

Javier

0 件の賞賛
返信

9,339件の閲覧回数
benlaj1
Contributor I

Hello @jgrijalba,

No, I did not try it, it is in my do to list. Can I just install the GPU driver from the W1.2.0 release onto the W1.1.0 that I already have or I should just start over from a clean W1.2.0 release?

Regards  

0 件の賞賛
返信

9,230件の閲覧回数
benlaj1
Contributor I
Hello, I've updated my setup with the 1.2.0 release (clean install) and still no GPU driver being loaded even though it should be based on the release notes. I also tried to install driver manually with the inf of galcore (both version m & mp) to no avail

Regards
0 件の賞賛
返信

9,471件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Could you show me the boot up log?

0 件の賞賛
返信

9,464件の閲覧回数
benlaj1
Contributor I

Hello @jimmychan,

Here's the boot log output you've requested:

 

Microsoft (R) Windows (R) Version 10.0 (Build 19041)
7 21 2022 05:44:39.796
BOOTLOG_LOADED \SystemRoot\system32\ntoskrnl.exe
BOOTLOG_LOADED \SystemRoot\system32\hal.dll
BOOTLOG_LOADED \SystemRoot\system32\kd.dll
BOOTLOG_LOADED \SystemRoot\System32\DriverStore\FileRepository\halextimxdma.inf_arm64_002b0bef7d780634\HalExtiMXDma.dll
BOOTLOG_LOADED \SystemRoot\System32\drivers\CLFS.SYS
BOOTLOG_LOADED \SystemRoot\System32\drivers\tm.sys
BOOTLOG_LOADED \SystemRoot\system32\PSHED.dll
BOOTLOG_LOADED \SystemRoot\system32\BOOTVID.dll
BOOTLOG_LOADED \SystemRoot\System32\drivers\FLTMGR.SYS
BOOTLOG_LOADED \SystemRoot\System32\drivers\msrpc.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\ksecdd.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\clipsp.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\cmimcext.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\werkernel.sys
BOOTLOG_LOADED \SystemRoot\system32\CI.dll
BOOTLOG_LOADED \SystemRoot\System32\drivers\cng.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\Wdf01000.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\WDFLDR.SYS
BOOTLOG_LOADED \SystemRoot\system32\drivers\WppRecorder.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\SleepStudyHelper.sys
BOOTLOG_LOADED \SystemRoot\System32\Drivers\acpiex.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\mssecflt.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\ACPI.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\WMILIB.SYS
BOOTLOG_LOADED \SystemRoot\system32\drivers\wd\WdBoot.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\WindowsTrustedRT.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\WindowsTrustedRTProxy.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\pcw.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\vdrvroot.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\pci.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\pdc.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\CEA.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\partmgr.sys
BOOTLOG_LOADED \SystemRoot\System32\Drivers\msgpioclx.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\spaceport.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\volmgr.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\volmgrx.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\sdbus.sys
BOOTLOG_LOADED \SystemRoot\System32\DriverStore\FileRepository\imxusdhc.inf_arm64_c2d099f02ee56325\imxusdhc.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\sdport.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\mountmgr.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\EhStorClass.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\fileinfo.sys
BOOTLOG_LOADED \SystemRoot\System32\Drivers\Wof.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\wd\WdFilter.sys
BOOTLOG_LOADED \SystemRoot\System32\Drivers\Ntfs.sys
BOOTLOG_LOADED \SystemRoot\System32\DriverStore\FileRepository\imxgpio.inf_arm64_34f8d54618e4d436\imxgpio.sys
BOOTLOG_LOADED \SystemRoot\System32\Drivers\Fs_Rec.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\ndis.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\NETIO.SYS
BOOTLOG_LOADED \SystemRoot\System32\Drivers\ksecpkg.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\tcpip.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\fwpkclnt.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\wfplwfs.sys
BOOTLOG_LOADED \SystemRoot\System32\DRIVERS\fvevol.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\volume.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\volsnap.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\sdstor.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\rdyboost.sys
BOOTLOG_LOADED \SystemRoot\System32\Drivers\mup.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\iorate.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\disk.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\CLASSPNP.SYS
BOOTLOG_LOADED \SystemRoot\System32\drivers\cdrom.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\filecrypt.sys
BOOTLOG_LOADED \SystemRoot\System32\Drivers\Null.SYS
BOOTLOG_LOADED \SystemRoot\System32\Drivers\Beep.SYS
BOOTLOG_LOADED \SystemRoot\System32\drivers\dxgkrnl.sys
BOOTLOG_NOT_LOADED \SystemRoot\System32\drivers\dxgkrnl.sys
BOOTLOG_LOADED \SystemRoot\System32\DriverStore\FileRepository\basicdisplay.inf_arm64_663991e43b981000\BasicDisplay.sys
BOOTLOG_NOT_LOADED \SystemRoot\System32\drivers\dxgkrnl.sys
BOOTLOG_LOADED \SystemRoot\System32\DriverStore\FileRepository\basicrender.inf_arm64_cddb4abef66c34c3\BasicRender.sys
BOOTLOG_LOADED \SystemRoot\System32\Drivers\Npfs.SYS
BOOTLOG_LOADED \SystemRoot\System32\Drivers\Msfs.SYS
BOOTLOG_LOADED \SystemRoot\System32\Drivers\CimFS.SYS
BOOTLOG_LOADED \SystemRoot\system32\DRIVERS\tdx.sys
BOOTLOG_LOADED \SystemRoot\System32\DRIVERS\netbt.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\afunix.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\afd.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\vwififlt.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\pacer.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\ndiscap.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\netbios.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\Vid.sys
BOOTLOG_LOADED \SystemRoot\system32\DRIVERS\rdbss.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\csc.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\nsiproxy.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\npsvctrig.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\mssmbios.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\gpuenergydrv.sys
BOOTLOG_LOADED \SystemRoot\System32\Drivers\dfsc.sys
BOOTLOG_LOADED \SystemRoot\System32\Drivers\fastfat.SYS
BOOTLOG_LOADED \SystemRoot\system32\drivers\dam.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\bam.sys
BOOTLOG_LOADED \SystemRoot\system32\DRIVERS\ahcache.sys
BOOTLOG_NOT_LOADED \SystemRoot\System32\drivers\dxgkrnl.sys
BOOTLOG_LOADED \SystemRoot\system32\DRIVERS\galcore.sys
BOOTLOG_LOADED \SystemRoot\System32\DriverStore\FileRepository\compositebus.inf_arm64_b97329ef45b32293\CompositeBus.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\kdnic.sys
BOOTLOG_LOADED \SystemRoot\System32\DriverStore\FileRepository\umbus.inf_arm64_bbb69c7f1ec57082\umbus.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\fxppm.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\ucx01000.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\USBXHCI.SYS
BOOTLOG_LOADED \SystemRoot\system32\drivers\SpbCx.sys
BOOTLOG_LOADED \SystemRoot\System32\DriverStore\FileRepository\imxecspi.inf_arm64_1e4ac6c444504002\imxecspi.sys
BOOTLOG_LOADED \SystemRoot\System32\DriverStore\FileRepository\imxi2c.inf_arm64_5dd632333ab1aef9\imxi2c.sys
BOOTLOG_LOADED \SystemRoot\System32\DriverStore\FileRepository\imxnetmini.inf_arm64_3ed6745d40d7287c\imxnetmini.sys
BOOTLOG_LOADED \SystemRoot\System32\DriverStore\FileRepository\imxaud.inf_arm64_3e4626a97bdd78ba\imxaud.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\ksthunk.sys
BOOTLOG_LOADED \SystemRoot\System32\DriverStore\FileRepository\opteetree.inf_arm64_324e5b6aca975d3c\OpteeTrEE.sys
BOOTLOG_LOADED \SystemRoot\System32\DriverStore\FileRepository\imxpwm.inf_arm64_ba0ff75f862899d5\imxpwm.sys
BOOTLOG_LOADED \SystemRoot\System32\DriverStore\FileRepository\imxthermalclient.inf_arm64_56f3aecd37b9f77d\imxthermalclient.sysBOOTLOG_LOADED \SystemRoot\System32\DriverStore\FileRepository\imxtmu.inf_arm64_adcfec7a3773d4a7\imxtmu.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\imxcan.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\NdisVirtualBus.sys
BOOTLOG_LOADED \SystemRoot\System32\DriverStore\FileRepository\swenum.inf_arm64_5a66725fb2fb215c\swenum.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\rdpbus.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\SerCx2.sys
BOOTLOG_LOADED \SystemRoot\System32\DriverStore\FileRepository\imxuart.inf_arm64_cbd279f21e21ec83\imxuart.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\rhproxy.sys
BOOTLOG_LOADED \SystemRoot\System32\Drivers\UcmCx.sys
BOOTLOG_LOADED \SystemRoot\System32\Drivers\UcmTcpciCx.sys
BOOTLOG_LOADED
BOOTLOG_LOADED \SystemRoot\System32\drivers\UsbHub3.sys
BOOTLOG_NOT_LOADED \SystemRoot\System32\drivers\WindowsTrustedRTProxy.sys
BOOTLOG_NOT_LOADED \SystemRoot\System32\drivers\WindowsTrustedRTProxy.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\usbccgp.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\hidusb.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\mouhid.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\mouclass.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\WindowsTrustedRTProxy.sys
BOOTLOG_NOT_LOADED \SystemRoot\System32\drivers\dxgkrnl.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\monitor.sys
BOOTLOG_NOT_LOADED \SystemRoot\System32\drivers\dxgkrnl.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\WUDFRd.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\rdpvideominiport.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\wcifs.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\rdpdr.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\luafv.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\cldflt.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\storqosflt.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\bindflt.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\WpdUpFltr.sys
BOOTLOG_LOADED \SystemRoot\system32\DRIVERS\bowser.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\msquic.sys
BOOTLOG_LOADED \SystemRoot\system32\DRIVERS\mrxsmb.sys
BOOTLOG_LOADED \SystemRoot\system32\DRIVERS\mrxsmb20.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\mslldp.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\tsusbhub.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\lltdio.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\rspndr.sys
BOOTLOG_LOADED \SystemRoot\System32\DRIVERS\wanarp.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\HTTP.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\mpsdrv.sys
BOOTLOG_LOADED \SystemRoot\System32\DRIVERS\srvnet.sys
BOOTLOG_LOADED \SystemRoot\System32\DRIVERS\srv2.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\mmcss.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\peauth.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\tcpipreg.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\Ndu.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\rassstp.sys
BOOTLOG_LOADED \SystemRoot\System32\DRIVERS\NDProxy.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\AgileVpn.sys
BOOTLOG_NOT_LOADED \SystemRoot\System32\DRIVERS\NDProxy.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\rasl2tp.sys
BOOTLOG_NOT_LOADED \SystemRoot\System32\DRIVERS\NDProxy.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\raspptp.sys
BOOTLOG_NOT_LOADED \SystemRoot\System32\DRIVERS\NDProxy.sys
BOOTLOG_LOADED \SystemRoot\System32\DRIVERS\raspppoe.sys
BOOTLOG_NOT_LOADED \SystemRoot\System32\DRIVERS\NDProxy.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\ndiswan.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\condrv.sys
BOOTLOG_NOT_LOADED \SystemRoot\system32\drivers\wd\WdFilter.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\wd\WdNisDrv.sys
BOOTLOG_NOT_LOADED \SystemRoot\System32\drivers\dxgkrnl.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\terminpt.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\kbdclass.sys
BOOTLOG_NOT_LOADED \SystemRoot\System32\drivers\dxgkrnl.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\IndirectKmd.sys

From what I see in the log, dxgkrnl.sys driver is not being loaded and basic display/renderer is loaded instead. 

Thanks for your support.

0 件の賞賛
返信

9,451件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Confirmed internally, the GPU is not supported yet on iMX8MP. The support will be added in the next release in September this year.

0 件の賞賛
返信

9,445件の閲覧回数
benlaj1
Contributor I

Hello @jimmychan,

Thanks for the confirmation. I'll wait for the next release in September and I'll try to remember to update this post once I've confirmed it to work with this future release.

Regards

0 件の賞賛
返信

9,234件の閲覧回数
benlaj1
Contributor I

Hello, I've updated my setup with the 1.2.0 release and still no GPU driver being loaded even though it should be based on the release notes.

 

On a side note, I noticed the procedure to deploy was a little bit different where prior 1.1.0 release you had to provide board name which is not there anymore in 1.2.0 and I encountered issues because of that while deploying in WinPE regarding the startnet.cmd/install.cmd command and disk creation scripts with diskpart...

Regards

タグ(1)
0 件の賞賛
返信

9,188件の閲覧回数
benlaj1
Contributor I
Hello @jimmychan, can you help? I seem to have the same boot log with 1.2.0 release as previous 1.1.0.
0 件の賞賛
返信

9,177件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Could you send me the boot log file?

0 件の賞賛
返信

9,174件の閲覧回数
benlaj1
Contributor I

Hello @jimmychan,

Here's the ntbtlog.txt content as requested:

Microsoft (R) Windows (R) Version 10.0 (Build 19041)
11 22 2022 05:25:42.574
BOOTLOG_LOADED \SystemRoot\system32\ntoskrnl.exe
BOOTLOG_LOADED \SystemRoot\system32\hal.dll
BOOTLOG_LOADED \SystemRoot\system32\kd.dll
BOOTLOG_LOADED \SystemRoot\System32\DriverStore\FileRepository\halextimxdma.inf_arm64_9a488cbe5f8b451b\HalExtiMXDma.dll
BOOTLOG_LOADED \SystemRoot\System32\drivers\CLFS.SYS
BOOTLOG_LOADED \SystemRoot\System32\drivers\tm.sys
BOOTLOG_LOADED \SystemRoot\system32\PSHED.dll
BOOTLOG_LOADED \SystemRoot\system32\BOOTVID.dll
BOOTLOG_LOADED \SystemRoot\System32\drivers\FLTMGR.SYS
BOOTLOG_LOADED \SystemRoot\System32\drivers\msrpc.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\ksecdd.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\clipsp.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\cmimcext.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\werkernel.sys
BOOTLOG_LOADED \SystemRoot\system32\CI.dll
BOOTLOG_LOADED \SystemRoot\System32\drivers\cng.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\Wdf01000.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\WDFLDR.SYS
BOOTLOG_LOADED \SystemRoot\system32\drivers\WppRecorder.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\SleepStudyHelper.sys
BOOTLOG_LOADED \SystemRoot\System32\Drivers\acpiex.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\mssecflt.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\ACPI.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\WMILIB.SYS
BOOTLOG_LOADED \SystemRoot\system32\drivers\WdBoot.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\WindowsTrustedRT.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\WindowsTrustedRTProxy.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\pcw.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\vdrvroot.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\pci.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\pdc.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\CEA.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\partmgr.sys
BOOTLOG_LOADED \SystemRoot\System32\Drivers\msgpioclx.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\spaceport.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\volmgr.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\volmgrx.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\sdbus.sys
BOOTLOG_LOADED \SystemRoot\System32\DriverStore\FileRepository\imxusdhc.inf_arm64_08dc04ef8f3ab51a\imxusdhc.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\sdport.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\mountmgr.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\EhStorClass.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\fileinfo.sys
BOOTLOG_LOADED \SystemRoot\System32\Drivers\Wof.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\WdFilter.sys
BOOTLOG_LOADED \SystemRoot\System32\Drivers\Ntfs.sys
BOOTLOG_LOADED \SystemRoot\System32\DriverStore\FileRepository\imxgpio.inf_arm64_e877bd6c6daa1b88\imxgpio.sys
BOOTLOG_LOADED \SystemRoot\System32\Drivers\Fs_Rec.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\ndis.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\NETIO.SYS
BOOTLOG_LOADED \SystemRoot\System32\Drivers\ksecpkg.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\tcpip.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\fwpkclnt.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\wfplwfs.sys
BOOTLOG_LOADED \SystemRoot\System32\DRIVERS\fvevol.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\volume.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\volsnap.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\sdstor.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\rdyboost.sys
BOOTLOG_LOADED \SystemRoot\System32\Drivers\mup.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\iorate.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\disk.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\CLASSPNP.SYS
BOOTLOG_LOADED \SystemRoot\System32\drivers\cdrom.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\filecrypt.sys
BOOTLOG_LOADED \SystemRoot\System32\Drivers\Null.SYS
BOOTLOG_LOADED \SystemRoot\System32\Drivers\Beep.SYS
BOOTLOG_LOADED \SystemRoot\System32\drivers\dxgkrnl.sys
BOOTLOG_NOT_LOADED \SystemRoot\System32\drivers\dxgkrnl.sys
BOOTLOG_LOADED \SystemRoot\System32\DriverStore\FileRepository\basicdisplay.inf_arm64_0013e8b29d941592\BasicDisplay.sys
BOOTLOG_NOT_LOADED \SystemRoot\System32\drivers\dxgkrnl.sys
BOOTLOG_LOADED \SystemRoot\System32\DriverStore\FileRepository\basicrender.inf_arm64_716851fb2d6a1523\BasicRender.sys
BOOTLOG_LOADED \SystemRoot\System32\Drivers\Npfs.SYS
BOOTLOG_LOADED \SystemRoot\System32\Drivers\Msfs.SYS
BOOTLOG_LOADED \SystemRoot\System32\Drivers\CimFS.SYS
BOOTLOG_LOADED \SystemRoot\system32\DRIVERS\tdx.sys
BOOTLOG_LOADED \SystemRoot\System32\DRIVERS\netbt.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\afunix.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\afd.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\vwififlt.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\pacer.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\ndiscap.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\netbios.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\Vid.sys
BOOTLOG_LOADED \SystemRoot\system32\DRIVERS\rdbss.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\csc.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\nsiproxy.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\npsvctrig.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\mssmbios.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\gpuenergydrv.sys
BOOTLOG_LOADED \SystemRoot\System32\Drivers\dfsc.sys
BOOTLOG_LOADED \SystemRoot\System32\Drivers\fastfat.SYS
BOOTLOG_LOADED \SystemRoot\system32\drivers\dam.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\bam.sys
BOOTLOG_LOADED \SystemRoot\system32\DRIVERS\ahcache.sys
BOOTLOG_LOADED \SystemRoot\System32\DriverStore\FileRepository\compositebus.inf_arm64_b97329ef45b32293\CompositeBus.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\kdnic.sys
BOOTLOG_LOADED \SystemRoot\System32\DriverStore\FileRepository\umbus.inf_arm64_bbb69c7f1ec57082\umbus.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\fxppm.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\ucx01000.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\USBXHCI.SYS
BOOTLOG_LOADED \SystemRoot\system32\drivers\SpbCx.sys
BOOTLOG_LOADED \SystemRoot\System32\DriverStore\FileRepository\imxecspi.inf_arm64_6295e90e05dccdb3\imxecspi.sys
BOOTLOG_LOADED \SystemRoot\System32\DriverStore\FileRepository\imxi2c.inf_arm64_c8bac581999acff9\imxi2c.sys
BOOTLOG_LOADED \SystemRoot\System32\DriverStore\FileRepository\imxnetmini.inf_arm64_94c80fa60ea12e06\imxnetmini.sys
BOOTLOG_LOADED \SystemRoot\System32\DriverStore\FileRepository\imxaud.inf_arm64_cda7abf44d128da0\imxaud.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\ksthunk.sys
BOOTLOG_LOADED \SystemRoot\System32\DriverStore\FileRepository\opteetree.inf_arm64_d92e58b3dbeb7150\OpteeTrEE.sys
BOOTLOG_LOADED \SystemRoot\System32\DriverStore\FileRepository\imxpwm.inf_arm64_df1ff7b1c4d06b3f\imxpwm.sys
BOOTLOG_LOADED \SystemRoot\System32\DriverStore\FileRepository\imxthermalclient.inf_arm64_c2b5a38aaa00676f\imxthermalclient.sysBOOTLOG_LOADED \SystemRoot\System32\DriverStore\FileRepository\imxtmu.inf_arm64_218609ce6833e5a7\imxtmu.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\imxcan.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\NdisVirtualBus.sys
BOOTLOG_LOADED \SystemRoot\System32\DriverStore\FileRepository\swenum.inf_arm64_5a66725fb2fb215c\swenum.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\rdpbus.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\SerCx2.sys
BOOTLOG_LOADED \SystemRoot\System32\DriverStore\FileRepository\imxuart.inf_arm64_776ffd56f12b044e\imxuart.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\rhproxy.sys
BOOTLOG_LOADED \SystemRoot\System32\Drivers\UcmCx.sys
BOOTLOG_LOADED \SystemRoot\System32\Drivers\UcmTcpciCx.sys
BOOTLOG_LOADED
BOOTLOG_LOADED \SystemRoot\System32\drivers\UsbHub3.sys
BOOTLOG_NOT_LOADED \SystemRoot\System32\drivers\WindowsTrustedRTProxy.sys
BOOTLOG_NOT_LOADED \SystemRoot\System32\drivers\WindowsTrustedRTProxy.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\hidusb.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\mouhid.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\mouclass.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\usbccgp.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\kbdhid.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\kbdclass.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\WindowsTrustedRTProxy.sys
BOOTLOG_NOT_LOADED \SystemRoot\System32\drivers\dxgkrnl.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\monitor.sys
BOOTLOG_NOT_LOADED \SystemRoot\System32\drivers\dxgkrnl.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\WUDFRd.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\rdpvideominiport.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\wcifs.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\luafv.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\cldflt.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\rdpdr.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\storqosflt.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\bindflt.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\WpdUpFltr.sys
BOOTLOG_LOADED \SystemRoot\system32\DRIVERS\bowser.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\msquic.sys
BOOTLOG_LOADED \SystemRoot\system32\DRIVERS\mrxsmb.sys
BOOTLOG_LOADED \SystemRoot\system32\DRIVERS\mrxsmb20.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\tsusbhub.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\mslldp.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\lltdio.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\rspndr.sys
BOOTLOG_LOADED \SystemRoot\System32\DRIVERS\wanarp.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\HTTP.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\mpsdrv.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\condrv.sys
BOOTLOG_LOADED \SystemRoot\System32\DRIVERS\srvnet.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\mmcss.sys
BOOTLOG_LOADED \SystemRoot\System32\DRIVERS\srv2.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\peauth.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\tcpipreg.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\Ndu.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\rassstp.sys
BOOTLOG_LOADED \SystemRoot\System32\DRIVERS\NDProxy.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\AgileVpn.sys
BOOTLOG_NOT_LOADED \SystemRoot\System32\DRIVERS\NDProxy.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\rasl2tp.sys
BOOTLOG_NOT_LOADED \SystemRoot\System32\DRIVERS\NDProxy.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\raspptp.sys
BOOTLOG_NOT_LOADED \SystemRoot\System32\DRIVERS\NDProxy.sys
BOOTLOG_LOADED \SystemRoot\System32\DRIVERS\raspppoe.sys
BOOTLOG_NOT_LOADED \SystemRoot\System32\DRIVERS\NDProxy.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\ndiswan.sys
BOOTLOG_NOT_LOADED \SystemRoot\system32\drivers\WdFilter.sys
BOOTLOG_LOADED \SystemRoot\system32\Drivers\WdNisDrv.sys
BOOTLOG_LOADED \SystemRoot\system32\Drivers\WdNisDrv.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\wd\WdFilter.sys
BOOTLOG_NOT_LOADED \SystemRoot\System32\drivers\dxgkrnl.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\terminpt.sys
BOOTLOG_NOT_LOADED \SystemRoot\System32\drivers\dxgkrnl.sys
BOOTLOG_LOADED \SystemRoot\System32\drivers\IndirectKmd.sys
BOOTLOG_LOADED \SystemRoot\system32\drivers\wd\WdNisDrv.sys

0 件の賞賛
返信

9,162件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

I am checking this with AE. I will update you when I get the reply.

0 件の賞賛
返信

9,132件の閲覧回数
benlaj1
Contributor I

Hello @jimmychan,

I can also add that my 8M Plus EVK board is using the MIPI-DSI interface with the IMX-MIPI-HDMI to have display output. I noticed this limitation in NXP W1.2.1 Release notes:

i.MX 8M Plus Limitation: MIPI-DSI display interface is not supported. When using MIPI-DSI
together with IMX-MIPI-HDMI, the booting image is displayed correctly, but as
soon as the Windows gpu driver is loaded, it changes to a black screen.
Workaround 1: Firmware support for MIPI-DSI is available, so boot the Windows
using LVDS display interface, uninstall GPU driver using Device Manager, reboot
Windows with the display connected to MIPI-DSI display interface.
Workaround 2: Prepare Windows installation without GPU driver. Download
Windows installation binaries, unzip them. Find and delete \IoTEntOnNXP\dri
vers\Galcore_mp_mn folder. Run the make-winpe-enterprise.cmd to
prepare the installation image. Apply the image to SD card, write firmware to the
SD card. Connect the display to MIPI-DSI display interface, install Windows and
reboot.

Could this be the reason I don't have the GPU loading? I did not do any of those workaround (I even tried to install the galcore driver manually to no avail). Should I try to get my hands on the IMX-LVDS-HDMI instead?

Regards

0 件の賞賛
返信

9,117件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Yes, the driver is in the \IoTEntOnNXP\drivers\Galcore_mp_mn folder.

0 件の賞賛
返信

9,110件の閲覧回数
benlaj1
Contributor I

Hello @jimmychan, as previously mentioned, trying to install it manually did nothing. Checking the setupapi.dev log file, it reports it doesn't find any matching devices. Here's the actual setupapi log when installing it :

>>> [Device Install (DiInstallDriver) - C:\Users\test\Desktop\drivers\Galcore_mp_mn\galcore.inf]
>>> Section start 2022/11/22 06:29:52.698
cmd: "C:\Windows\System32\InfDefaultInstall.exe" "C:\Users\test\Desktop\drivers\Galcore_mp_mn\galcore.inf"
ndv: Flags: 0x00000000
ndv: INF path: C:\Users\test\Desktop\drivers\Galcore_mp_mn\galcore.inf
dvs: {DrvSetupInstallDriver - C:\Users\test\Desktop\drivers\Galcore_mp_mn\galcore.inf}
dvs: Flags: 0x00000000
dvs: {Driver Setup Import Driver Package: C:\Users\test\Desktop\drivers\Galcore_mp_mn\galcore.inf} 06:29:52.745
sto: {Copy Driver Package: C:\Users\test\Desktop\drivers\Galcore_mp_mn\galcore.inf} 06:29:52.792
sto: Driver Package = C:\Users\test\Desktop\drivers\Galcore_mp_mn\galcore.inf
sto: Flags = 0x00000007
sto: Destination = C:\Users\test\AppData\Local\Temp\{032f75d8-e563-2148-93b6-a94625d1ec38}
sto: Copying driver package files to 'C:\Users\test\AppData\Local\Temp\{032f75d8-e563-2148-93b6-a94625d1ec38}'.
flq: {FILE_QUEUE_COMMIT} 06:29:52.839
flq: Copying 'C:\Users\test\Desktop\drivers\Galcore_mp_mn\vulkan.dll' to 'C:\Users\test\AppData\Local\Temp\{032f75d8-e563-2148-93b6-a94625d1ec38}\vulkan.dll'.
flq: Copying 'C:\Users\test\Desktop\drivers\Galcore_mp_mn\galcore.cat' to 'C:\Users\test\AppData\Local\Temp\{032f75d8-e563-2148-93b6-a94625d1ec38}\galcore.cat'.
flq: Copying 'C:\Users\test\Desktop\drivers\Galcore_mp_mn\galcore.inf' to 'C:\Users\test\AppData\Local\Temp\{032f75d8-e563-2148-93b6-a94625d1ec38}\galcore.inf'.
flq: Copying 'C:\Users\test\Desktop\drivers\Galcore_mp_mn\galcore.sys' to 'C:\Users\test\AppData\Local\Temp\{032f75d8-e563-2148-93b6-a94625d1ec38}\galcore.sys'.
flq: Copying 'C:\Users\test\Desktop\drivers\Galcore_mp_mn\libGAL_32.dll' to 'C:\Users\test\AppData\Local\Temp\{032f75d8-e563-2148-93b6-a94625d1ec38}\libGAL_32.dll'.
flq: Copying 'C:\Users\test\Desktop\drivers\Galcore_mp_mn\spvconverter.dll' to 'C:\Users\test\AppData\Local\Temp\{032f75d8-e563-2148-93b6-a94625d1ec38}\spvconverter.dll'.
flq: Copying 'C:\Users\test\Desktop\drivers\Galcore_mp_mn\libVSC_32.dll' to 'C:\Users\test\AppData\Local\Temp\{032f75d8-e563-2148-93b6-a94625d1ec38}\libVSC_32.dll'.
flq: Copying 'C:\Users\test\Desktop\drivers\Galcore_mp_mn\libGLSLC.dll' to 'C:\Users\test\AppData\Local\Temp\{032f75d8-e563-2148-93b6-a94625d1ec38}\libGLSLC.dll'.
flq: Copying 'C:\Users\test\Desktop\drivers\Galcore_mp_mn\vulkan_32.dll' to 'C:\Users\test\AppData\Local\Temp\{032f75d8-e563-2148-93b6-a94625d1ec38}\vulkan_32.dll'.
flq: Copying 'C:\Users\test\Desktop\drivers\Galcore_mp_mn\umd11.dll' to 'C:\Users\test\AppData\Local\Temp\{032f75d8-e563-2148-93b6-a94625d1ec38}\umd11.dll'.
flq: Copying 'C:\Users\test\Desktop\drivers\Galcore_mp_mn\spvconverter_32.dll' to 'C:\Users\test\AppData\Local\Temp\{032f75d8-e563-2148-93b6-a94625d1ec38}\spvconverter_32.dll'.
flq: Copying 'C:\Users\test\Desktop\drivers\Galcore_mp_mn\libGLSLC_32.dll' to 'C:\Users\test\AppData\Local\Temp\{032f75d8-e563-2148-93b6-a94625d1ec38}\libGLSLC_32.dll'.
flq: Copying 'C:\Users\test\Desktop\drivers\Galcore_mp_mn\libGAL.dll' to 'C:\Users\test\AppData\Local\Temp\{032f75d8-e563-2148-93b6-a94625d1ec38}\libGAL.dll'.
flq: Copying 'C:\Users\test\Desktop\drivers\Galcore_mp_mn\umd11_32.dll' to 'C:\Users\test\AppData\Local\Temp\{032f75d8-e563-2148-93b6-a94625d1ec38}\umd11_32.dll'.
flq: Copying 'C:\Users\test\Desktop\drivers\Galcore_mp_mn\libVSC.dll' to 'C:\Users\test\AppData\Local\Temp\{032f75d8-e563-2148-93b6-a94625d1ec38}\libVSC.dll'.
flq: {FILE_QUEUE_COMMIT - exit(0x00000000)} 06:29:55.151
sto: {Copy Driver Package: exit(0x00000000)} 06:29:55.167
ump: Import flags: 0x00000000
pol: {Driver package policy check} 06:29:55.323
pol: {Driver package policy check - exit(0x00000000)} 06:29:55.323
sto: {Stage Driver Package: C:\Users\test\AppData\Local\Temp\{032f75d8-e563-2148-93b6-a94625d1ec38}\galcore.inf} 06:29:55.339
inf: {Query Configurability: C:\Users\test\AppData\Local\Temp\{032f75d8-e563-2148-93b6-a94625d1ec38}\galcore.inf} 06:29:55.370
! inf: Found legacy AddReg operation using non-relative key (HKLM\SOFTWARE\Microsoft\XAML). Code = 1304
! inf: Driver package 'galcore.inf' is NOT configurable.
inf: {Query Configurability: exit(0x00000000)} 06:29:55.386
flq: {FILE_QUEUE_COMMIT} 06:29:55.401
flq: Copying 'C:\Users\test\AppData\Local\Temp\{032f75d8-e563-2148-93b6-a94625d1ec38}\vulkan.dll' to 'C:\Windows\System32\DriverStore\Temp\{1c99729c-0f59-7145-9c58-3f731b138b33}\vulkan.dll'.
flq: Copying 'C:\Users\test\AppData\Local\Temp\{032f75d8-e563-2148-93b6-a94625d1ec38}\galcore.cat' to 'C:\Windows\System32\DriverStore\Temp\{1c99729c-0f59-7145-9c58-3f731b138b33}\galcore.cat'.
flq: Copying 'C:\Users\test\AppData\Local\Temp\{032f75d8-e563-2148-93b6-a94625d1ec38}\galcore.inf' to 'C:\Windows\System32\DriverStore\Temp\{1c99729c-0f59-7145-9c58-3f731b138b33}\galcore.inf'.
flq: Copying 'C:\Users\test\AppData\Local\Temp\{032f75d8-e563-2148-93b6-a94625d1ec38}\galcore.sys' to 'C:\Windows\System32\DriverStore\Temp\{1c99729c-0f59-7145-9c58-3f731b138b33}\galcore.sys'.
flq: Copying 'C:\Users\test\AppData\Local\Temp\{032f75d8-e563-2148-93b6-a94625d1ec38}\libGAL_32.dll' to 'C:\Windows\System32\DriverStore\Temp\{1c99729c-0f59-7145-9c58-3f731b138b33}\libGAL_32.dll'.
flq: Copying 'C:\Users\test\AppData\Local\Temp\{032f75d8-e563-2148-93b6-a94625d1ec38}\spvconverter.dll' to 'C:\Windows\System32\DriverStore\Temp\{1c99729c-0f59-7145-9c58-3f731b138b33}\spvconverter.dll'.
flq: Copying 'C:\Users\test\AppData\Local\Temp\{032f75d8-e563-2148-93b6-a94625d1ec38}\libVSC_32.dll' to 'C:\Windows\System32\DriverStore\Temp\{1c99729c-0f59-7145-9c58-3f731b138b33}\libVSC_32.dll'.
flq: Copying 'C:\Users\test\AppData\Local\Temp\{032f75d8-e563-2148-93b6-a94625d1ec38}\libGLSLC.dll' to 'C:\Windows\System32\DriverStore\Temp\{1c99729c-0f59-7145-9c58-3f731b138b33}\libGLSLC.dll'.
flq: Copying 'C:\Users\test\AppData\Local\Temp\{032f75d8-e563-2148-93b6-a94625d1ec38}\vulkan_32.dll' to 'C:\Windows\System32\DriverStore\Temp\{1c99729c-0f59-7145-9c58-3f731b138b33}\vulkan_32.dll'.
flq: Copying 'C:\Users\test\AppData\Local\Temp\{032f75d8-e563-2148-93b6-a94625d1ec38}\umd11.dll' to 'C:\Windows\System32\DriverStore\Temp\{1c99729c-0f59-7145-9c58-3f731b138b33}\umd11.dll'.
flq: Copying 'C:\Users\test\AppData\Local\Temp\{032f75d8-e563-2148-93b6-a94625d1ec38}\spvconverter_32.dll' to 'C:\Windows\System32\DriverStore\Temp\{1c99729c-0f59-7145-9c58-3f731b138b33}\spvconverter_32.dll'.
flq: Copying 'C:\Users\test\AppData\Local\Temp\{032f75d8-e563-2148-93b6-a94625d1ec38}\libGLSLC_32.dll' to 'C:\Windows\System32\DriverStore\Temp\{1c99729c-0f59-7145-9c58-3f731b138b33}\libGLSLC_32.dll'.
flq: Copying 'C:\Users\test\AppData\Local\Temp\{032f75d8-e563-2148-93b6-a94625d1ec38}\libGAL.dll' to 'C:\Windows\System32\DriverStore\Temp\{1c99729c-0f59-7145-9c58-3f731b138b33}\libGAL.dll'.
flq: Copying 'C:\Users\test\AppData\Local\Temp\{032f75d8-e563-2148-93b6-a94625d1ec38}\umd11_32.dll' to 'C:\Windows\System32\DriverStore\Temp\{1c99729c-0f59-7145-9c58-3f731b138b33}\umd11_32.dll'.
flq: Copying 'C:\Users\test\AppData\Local\Temp\{032f75d8-e563-2148-93b6-a94625d1ec38}\libVSC.dll' to 'C:\Windows\System32\DriverStore\Temp\{1c99729c-0f59-7145-9c58-3f731b138b33}\libVSC.dll'.
flq: {FILE_QUEUE_COMMIT - exit(0x00000000)} 06:29:56.917
sto: {DRIVERSTORE IMPORT VALIDATE} 06:29:56.932
sig: Driver package catalog is valid.
sig: {_VERIFY_FILE_SIGNATURE} 06:29:57.026
sig: Key = galcore.inf
sig: FilePath = C:\Windows\System32\DriverStore\Temp\{1c99729c-0f59-7145-9c58-3f731b138b33}\galcore.inf
sig: Catalog = C:\Windows\System32\DriverStore\Temp\{1c99729c-0f59-7145-9c58-3f731b138b33}\galcore.cat
sig: Success: File is signed in catalog.
sig: {_VERIFY_FILE_SIGNATURE exit(0x00000000)} 06:29:57.198
sto: {DRIVERSTORE IMPORT VALIDATE: exit(0x00000000)} 06:29:59.073
sig: Signer Score = 0x0D000005 (WHQL)
sig: Signer Name = Microsoft Windows Hardware Compatibility Publisher
sig: Submission ID = 30043800_14067914596444528_1152921505695397261
sto: {Core Driver Package Import: galcore.inf_arm64_8ae056a8bccf916f} 06:29:59.089
sto: {DRIVERSTORE IMPORT BEGIN} 06:29:59.104
sto: {DRIVERSTORE IMPORT BEGIN: exit(0x00000000)} 06:29:59.104
cpy: {Copy Directory: C:\Windows\System32\DriverStore\Temp\{1c99729c-0f59-7145-9c58-3f731b138b33}} 06:29:59.104
cpy: Target Path = C:\Windows\System32\DriverStore\FileRepository\galcore.inf_arm64_8ae056a8bccf916f
cpy: {Copy Directory: exit(0x00000000)} 06:29:59.167
idb: {Register Driver Package: C:\Windows\System32\DriverStore\FileRepository\galcore.inf_arm64_8ae056a8bccf916f\galcore.inf} 06:29:59.167
idb: Created driver package object 'galcore.inf_arm64_8ae056a8bccf916f' in DRIVERS database node.
idb: Created driver INF file object 'oem2.inf' in DRIVERS database node.
idb: Registered driver package 'galcore.inf_arm64_8ae056a8bccf916f' with 'oem2.inf'.
idb: {Register Driver Package: exit(0x00000000)} 06:29:59.198
idb: {Publish Driver Package: C:\Windows\System32\DriverStore\FileRepository\galcore.inf_arm64_8ae056a8bccf916f\galcore.inf} 06:29:59.198
idb: Activating driver package 'galcore.inf_arm64_8ae056a8bccf916f'.
cpy: Published 'galcore.inf_arm64_8ae056a8bccf916f\galcore.inf' to 'oem2.inf'.
idb: Indexed 3 device IDs for 'galcore.inf_arm64_8ae056a8bccf916f'.
sto: Flushed driver database node 'DRIVERS'. Time = 32 ms
sto: Flushed driver database node 'SYSTEM'. Time = 93 ms
idb: {Publish Driver Package: exit(0x00000000)} 06:29:59.386
sto: {DRIVERSTORE IMPORT END} 06:29:59.401
dvi: Flushed all driver package files to disk. Time = 1203 ms
sig: Installed catalog 'galcore.cat' as 'oem2.cat'.
sto: {DRIVERSTORE IMPORT END: exit(0x00000000)} 06:30:00.651
sto: {Core Driver Package Import: exit(0x00000000)} 06:30:00.651
sto: {Stage Driver Package: exit(0x00000000)} 06:30:00.682
dvs: {Driver Setup Import Driver Package - exit (0x00000000)} 06:30:00.870
! dvs: Unable to find any matching devices.
dvs: {DrvSetupInstallDriver - exit(00000000)}
<<< Section end 2022/11/22 06:30:00.917
<<< [Exit status: SUCCESS]

0 件の賞賛
返信

9,049件の閲覧回数
benlaj1
Contributor I

Hello @jimmychan

Do you have any news from your AE? I do not have any solution yet for GPU driver not loading with i.MX8M Plus EVK board.

Please keep me posted.

Regards

0 件の賞賛
返信