GPU accelerated browser

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPU accelerated browser

2,264件の閲覧回数
bharadwaaj
Contributor III

Hi all,

   I have a graphic intensive application which has to be run on the browser in kiosk mode in linux. So far tested with crhomium in i.MX6 dl sabreauto. Please let me know which browser supports GPU acceleration and do i need to do any configurations for the same.

Thanks in advance...

タグ(3)
0 件の賞賛
返信
1 返信

1,994件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI Bharadwaaj

for browsers please look at attached Yocto Guide from L3.14.28_1.0.0_iMX6QDLS_BUNDLE

sect.5.6.6 Chromium Browser on X11 and Wayland

sect.5.6.7 Qt5 and WebKit browser

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信