GPU Version info

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPU Version info

6,575 Views
sunishm
Contributor I

Hi Freescale

For Kernel -3.10.31 : GPU Version is 5.0.11P1 which is the part of KK 4.4.3  android release.


I would like to know the GPU Version for the KK 4.4.2 android release with the Kernel-3.0.35

Regards,

Sunish.M

0 Kudos
Reply
5 Replies

6,323 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

Would be possible that you tell me the part number that you are using?

Regards

Vicente

0 Kudos
Reply

6,321 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sunish

kernel-3.0.35 uses gpu 4.6.9 p12 version,

as shown in attached doc p.4.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

6,321 Views
sunishm
Contributor I

Thanks igor

0 Kudos
Reply

6,321 Views
sunishm
Contributor I

Hi ,

Please find the part no MCIMX6L3DVN10AA

0 Kudos
Reply

6,321 Views
vicentegomez
NXP TechSupport
NXP TechSupport

I will move your Thread to the IMX team.

Regards

Vicente

0 Kudos
Reply