GPU Stress test in imx8qxp

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPU Stress test in imx8qxp

904件の閲覧回数
arunsathian
Contributor III

Hi NXP ,


I need to stress the gpu and I found that glmark2 utility is used to stress the gpu from the NXP forum itself, and I just enabled it in the board. glmark2-es2 , glmark-es2-drm , glmark-es2 -wayland , these 3 utilities showing. Among these which should I prefer and can you please provide the commands needed.

0 件の賞賛
返信
1 返信

885件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @arunsathian 

 

glmark2-es2 is the standard version that uses OpenGL ES 2.0 and typically runs in an X11 environment.

glmark2-es2-drm runs directly on the Direct Rendering Manager (DRM) without a windowing system like X11 or Wayland.

glmark2-es2-wayland runs in a Wayland environment.

 

For example, running glmark2-es2-wayland will start the benchmark and display various performance tests on the screen. The results will be printed in the terminal once all tests are complete.

 

Also it s helpful run glmark2-es2-wayland --help

 

Best regards,

--... ...--

Salas.

0 件の賞賛
返信