GPU Ctx Init Failed - trying to enable hw acceleration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPU Ctx Init Failed - trying to enable hw acceleration

ソリューションへジャンプ
6,181件の閲覧回数
oskar
Contributor II

Board - i.MX6Q SD + "i.MX 6Dual/6Quad Linux Reference Manual" - Chapter 12 - X Windows Acceleration.

 

In xorg.conf, if I set "fbdev" as Driver in section "Device" - system is starting, hardware acceleration is not available.

 

I installed gpu-viv-bin-mx6q_12.09.01-1_armel.deb and xserver-xorg-video-imx-viv_12.09.01-1_armel.deb. The xorg.conf file has been changed - "vivante" as Driver. The content looks similar to the description in "12.3.4 xorg.conf for i.MX 6".

Unfortunately the result is different than I expected - screen is black. Also in Xorg.0.log I see some errors:

 

[   161.393] (II) VIVANTE(0): test Initializing EXA

[   161.394] (EE) VIVANTE(0): internal error: GPU Ctx Init Failed

[   161.394] (EE) VIVANTE(0): internal error: initExaLayer failed in VivScreenInit()

[   161.394] (==) VIVANTE(0): Backing store disabled

[   161.404] (==) VIVANTE(0): DPMS enabled

[   161.874] [drm] failed to load kernel module "vivante"

[   161.874] (EE) VIVANTE(0): [dri] DRIScreenInit failed.  Disabling DRI.

 

Unfortunately I cannot find solution or reason of the problem.

 

Original Attachment has been moved to: Xorg.log.zip

ラベル(4)
1 解決策
3,279件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

Employee

I verified with the PostGA release, it i loading good, no more error. Make sure kernel modules installed to the rootfs. Below is the log

843] (II) VIVANTE(0): FB Start = 0x3318b000  FB Base = 0x3318b000  FB Offset = (nil)

[    23.861] (II) VIVANTE(0): test Initializing EXA

[    23.861] (II) EXA(0): Driver allocated offscreen pixmaps

[    23.861] (II) EXA(0): Driver registered support for the following operations:

[    23.861] (II)         Solid

[    23.861] (II)         Copy

[    23.861] (II)         Composite (RENDER acceleration)

[    23.861] (II)         UploadToScreen

[    23.881] (==) VIVANTE(0): Backing store disabled

[    23.892] (==) VIVANTE(0): DPMS enabled

[    23.893] drmOpenDevice: node name is /dev/dri/card0

[    23.899] drmOpenDevice: node name is /dev/dri/card0

[    24.078] drmOpenByBusid: Searching for BusID platform:Vivante GCCore

[    24.078] drmOpenDevice: node name is /dev/dri/card0

[    24.078] drmOpenDevice: open result is 12, (OK)

[    24.078] drmOpenByBusid: drmOpenMinor returns 12

[    24.078] drmOpenByBusid: drmGetBusid reports platform:Vivante GCCore

[    24.079] (II) [drm] loaded kernel module for "vivante" driver.

[    24.079] (II) [drm] DRM interface version 1.4

[    24.079] (II) [drm] DRM open master succeeded.

[    24.079] (II) VIVANTE(0): [drm] Using the DRM lock SAREA also for drawables.

[    24.079] (II) VIVANTE(0): [drm] framebuffer handle = 0x18000000

[    24.079] (II) VIVANTE(0): [drm] added 1 reserved context for kernel

[    24.079] (II) VIVANTE(0): X context handle = 0x1

[    24.080] (II) VIVANTE(0): [drm] installed DRM signal handler

[    24.080] (II) VIVANTE(0): [DRI] installation complete

[    24.080] (==) RandR enabled

元の投稿で解決策を見る

3 返答(返信)
3,279件の閲覧回数
N_Coesel
Contributor III

The problem is that the libraries from Freescale don't support hard floating point. Timesys had made GPU libraries with hard floating point support. I still don't manage to get X working but at least the crash is resolved.

0 件の賞賛
返信
3,280件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

Employee

I verified with the PostGA release, it i loading good, no more error. Make sure kernel modules installed to the rootfs. Below is the log

843] (II) VIVANTE(0): FB Start = 0x3318b000  FB Base = 0x3318b000  FB Offset = (nil)

[    23.861] (II) VIVANTE(0): test Initializing EXA

[    23.861] (II) EXA(0): Driver allocated offscreen pixmaps

[    23.861] (II) EXA(0): Driver registered support for the following operations:

[    23.861] (II)         Solid

[    23.861] (II)         Copy

[    23.861] (II)         Composite (RENDER acceleration)

[    23.861] (II)         UploadToScreen

[    23.881] (==) VIVANTE(0): Backing store disabled

[    23.892] (==) VIVANTE(0): DPMS enabled

[    23.893] drmOpenDevice: node name is /dev/dri/card0

[    23.899] drmOpenDevice: node name is /dev/dri/card0

[    24.078] drmOpenByBusid: Searching for BusID platform:Vivante GCCore

[    24.078] drmOpenDevice: node name is /dev/dri/card0

[    24.078] drmOpenDevice: open result is 12, (OK)

[    24.078] drmOpenByBusid: drmOpenMinor returns 12

[    24.078] drmOpenByBusid: drmGetBusid reports platform:Vivante GCCore

[    24.079] (II) [drm] loaded kernel module for "vivante" driver.

[    24.079] (II) [drm] DRM interface version 1.4

[    24.079] (II) [drm] DRM open master succeeded.

[    24.079] (II) VIVANTE(0): [drm] Using the DRM lock SAREA also for drawables.

[    24.079] (II) VIVANTE(0): [drm] framebuffer handle = 0x18000000

[    24.079] (II) VIVANTE(0): [drm] added 1 reserved context for kernel

[    24.079] (II) VIVANTE(0): X context handle = 0x1

[    24.080] (II) VIVANTE(0): [drm] installed DRM signal handler

[    24.080] (II) VIVANTE(0): [DRI] installation complete

[    24.080] (==) RandR enabled

3,279件の閲覧回数
kevincheng
Contributor IV

We've the same issue in L3.0.35_4.0.0_UBUNTU_RFS.

Have any one have solution?

0 件の賞賛
返信