GPT Input Capture Linux Driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPT Input Capture Linux Driver

ソリューションへジャンプ
4,013件の閲覧回数
aliismail
Contributor IV

I am running on an iMX6QDL and I would like to configure the GPT input capture channels. I have not located any Linux drivers that allow me to configure the GPT registers and read the count register. I have seen the imx6-gpt driver and it doesn't seem to do much other than set the clocks and enable the interrupt. I would like to configure the input channels as well. Anyone have any thoughts on how to achieve this?

ラベル(2)
0 件の賞賛
返信
1 解決策
3,592件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ali

one can look on timer-imx-gpt.c

[27/38] clocksource/drivers/imx: add input capture support - Patchwork 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,593件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ali

one can look on timer-imx-gpt.c

[27/38] clocksource/drivers/imx: add input capture support - Patchwork 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,592件の閲覧回数
aliismail
Contributor IV

Thanks a lot Igor! Do you happen to know if there is a more updated patch?

0 件の賞賛
返信