GPT DBGEN Bit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPT DBGEN Bit

2,149 Views
sohaib_sulehri
Contributor I

According to iMX8QM_RM_Rev_E Section 7.10.4.2.5:
If DBGEN bit is not set for GPT_CR register then GPT timer is halted.
But in my case GPT Timer counter continue running even though DBGEN is 0 and code execution is stopped using debugger. 
What could be the reason?

0 Kudos
Reply
1 Reply

2,085 Views
b36401
NXP Employee
NXP Employee

In debug mode, PWM has the option of continuing to run or be halted.
If the DBGEN bit is not set in the PWM_PWMCR, the PWM is halted.
If the DBGEN bit is set, then the PWM will continue to run in the debug mode.

0 Kudos
Reply