GPT DBGEN Bit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPT DBGEN Bit

2,204件の閲覧回数
sohaib_sulehri
Contributor I

According to iMX8QM_RM_Rev_E Section 7.10.4.2.5:
If DBGEN bit is not set for GPT_CR register then GPT timer is halted.
But in my case GPT Timer counter continue running even though DBGEN is 0 and code execution is stopped using debugger. 
What could be the reason?

ラベル(1)
0 件の賞賛
返信
1 返信

2,140件の閲覧回数
b36401
NXP Employee
NXP Employee

In debug mode, PWM has the option of continuing to run or be halted.
If the DBGEN bit is not set in the PWM_PWMCR, the PWM is halted.
If the DBGEN bit is set, then the PWM will continue to run in the debug mode.

0 件の賞賛
返信