GPS on IMX6SL ICS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPS on IMX6SL ICS

2,941 Views
raghavendraning
Contributor I

Hi,

I am using uart interface for GPS in my imx6sl.cat /dev/ttymxc works fine .From my any of the android gps-apps i could't able to receive data.

But in my logcat i could able to get NMEA data from my HAL lib gps.default.so

I am using

HAL-->gps.default.so(which i compiled by gps_serial.c)

In BoardConfig.mk--->

BOARD_HAVE_HARDWARE_GPS := true

USE_NMEA_GPS_HARDWARE := true

Can any one help me to fix this issue.

Labels (3)
Tags (3)
0 Kudos
Reply
3 Replies

2,362 Views
raghavendraning
Contributor I

Hi Arulpandiyan,

Yeah.It has been solved.I used some other gps libraries.

0 Kudos
Reply

2,362 Views
eric_kang
Contributor II

Dear raghavendra ningoji,

I have the same problem in i.MX7D/Android M6.0.1.

Could you share the detailed method?

I'll send the message with my e-mail address to you.

0 Kudos
Reply

2,362 Views
balashanmugam
Contributor III

hi raghav,

     Have you solved this issue, If you solved can you pls share the details, we are also facing the same kind of issue in our module.

Regards

Arulpandiyan V

0 Kudos
Reply