Setting gstreamer default audio as imx-hdmi-soc instead of wm8962-audio to

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Setting gstreamer default audio as imx-hdmi-soc instead of wm8962-audio to

1,102件の閲覧回数
greatcatchen
Contributor I

EVK:imx6q-sabresd
OS:Linux 3.1.53
image:fsl-image-qt5-x11-imx6qdlsolo.sdcard

etc/gconf/gconf.xml.defaults/schemas/system/gstreamer/0.10/default/%gconf.xml
etc/gconf/schemas/gstreamer-0.10.schemas

change form
<default>autoaudiosink</default>
to
<default>autoaudiosink device=hw:1</default>

Is there any better way ?

ラベル(2)
0 件の賞賛
返信
1 返信

941件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

The following may help.

https://community.nxp.com/docs/DOC-93745 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信