GPMI read nand flash ID

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPMI read nand flash ID

2,607件の閲覧回数
michaelsyh
Contributor I

I want to read the nand flash ID through GPMI,I write the 0x90(read ID command)and the address,I wonder if performing effectively, which register will show the expected ID(5 bytes), gpmi_data or gpmi_payload register,should I enable the gpmi_eccctrl register?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,432件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  ID data will be located in DMA buffer (DRAM).

You may look at the Platform SDK example. Unfortunately the SDK

is not supported more and it cannot be loaded from the NXP Web.

You may create request to get the SDK.

How to submit a new question for NXP Support

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,432件の閲覧回数
michaelsyh
Contributor I

Hello!DMA buffer is the APBH-CHn-BAR register, right? I can not find where DRAM is, so this process does not need to involve BCH,and does not need to enable the gpmi-eccctrl?

really appreciate your reply!!!thanks a lot!

发自我的 iPhone

在 2016年4月22日,下午2:41,Yuri <[email protected]> 写道:

NXP Community

GPMI read nand flash ID

reply from Yuri Muhin in i.MX Community - View the full discussion

Hello,

ID data will be located in DMA buffer (DRAM).

You may look at the Platform SDK example. Unfortunately the SDK

is not supported more and it cannot be loaded from the NXP Web.

You may create request to get the SDK.

How to submit a new question for NXP Support

Have a great day,

Yuri

>

0 件の賞賛
返信

2,432件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

Please try the GPMI example from the Platform SDK.

Regards,

Yuri.

0 件の賞賛
返信