GPMI Documentation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
7,735件の閲覧回数
briannorman
Contributor II

Is there any documentation or reference manual for the GPMI module on the IMX6?  I have the iMX6 ref manual, but the GPMI section is lacking any documentation on how to use it.  I'm creating a driver in Green Hills and without the linux libraries, the linux drivers are not too helpful.  All i need to do is interface existing ONFI board interface calls with the GPMI controller, ie send_cmd, write_page, read_page, etc. 

ラベル(2)
0 件の賞賛
返信
1 解決策
5,935件の閲覧回数
Yuri
NXP Employee
NXP Employee

There is no much additional information about the GPMI, nevertheless

the following may be helpful.

https://community.freescale.com/message/379149#379149

Also, please refer to examples in the Platform SDK. Please take a look at

Chapter 13 (Configuring the GPMI Controller) of "iMX6_Firmware_Guide.pdf".

The SDK link :

"Bare-metal SDK for the i.MX 6 series, including reusable drivers and tests for

many peripherals, and much example code. Also includes register definition

headers files, and register definitions for debuggers"

https://www.freescale.com/webapp/Download?colCode=i.MX6_PLATFORM_SDK&location=null


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
5,936件の閲覧回数
Yuri
NXP Employee
NXP Employee

There is no much additional information about the GPMI, nevertheless

the following may be helpful.

https://community.freescale.com/message/379149#379149

Also, please refer to examples in the Platform SDK. Please take a look at

Chapter 13 (Configuring the GPMI Controller) of "iMX6_Firmware_Guide.pdf".

The SDK link :

"Bare-metal SDK for the i.MX 6 series, including reusable drivers and tests for

many peripherals, and much example code. Also includes register definition

headers files, and register definitions for debuggers"

https://www.freescale.com/webapp/Download?colCode=i.MX6_PLATFORM_SDK&location=null


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
5,935件の閲覧回数
briannorman
Contributor II

where can i find the "iMX6_Firmware_Guide.pdf"?

0 件の賞賛
返信
5,935件の閲覧回数
Yuri
NXP Employee
NXP Employee

The Platform SDK, linked earlier, contains doc folder. 

0 件の賞賛
返信