GPIO synchrization with an external clock signal

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPIO synchrization with an external clock signal

1,110件の閲覧回数
pratham_malaviya
Contributor III
Dear All,
 

We are planning to interface the AD4134 ADC with the i.MX8MP processor. The ADC operates with its own clock, which can go up to a maximum of 48 MHz, and the digital data is output in sync with this clock.

We intend to use a general-purpose GPIO pin on the i.MX8MP to capture the digital data, but it is critical that the GPIO operations are synchronized with the clock signal provided by the ADC.

In this context, we have the following queries:

  1. Is it possible to synchronize a GPIO pin with an external clock?
  2. How can we interface the ADC clock with the i.MX8MP processor, and what configurations are necessary to ensure proper synchronization between the clock and the GPIO?

We would appreciate any guidance or suggestions regarding the best approach to achieve this synchronization.

タグ(4)
0 件の賞賛
返信
1 返信

1,092件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @pratham_malaviya 

As a suggestion, you can use the Cortex M core inside of the i.MX8MP to Sync the external clock of your ADC module with an IRQ and read the data in the same IRQ.

If you need to get the values obtained by the ADC to the Linux OS, you can share the obtained values thorough RPMSG.

Best regards,

Salas.

0 件の賞賛
返信