GPIO request_threaded_irq sample

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPIO request_threaded_irq sample

1,403 Views
tzeng015
Contributor II

Hi all

platform : imx8mm

Linux : 5-10

I want to test my GPIO (GPIO4_14) via request_threaded_irq . I want to make sure this pin can accept interrupt OK.

Do you have any sample ?

0 Kudos
Reply
1 Reply

1,384 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @tzeng015,

Refer to this link for more information.

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

 

Thanks & Regards,
Dhruvit.

0 Kudos
Reply