GPIO interrupt configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPIO interrupt configuration

1,398 Views
ashokp
Contributor I

Hi all,

I am working on IMX6Q based custom board. I am using android kitkat and kernel 3.0.35 (No device tree support)

In my design we are using a PCA9535AHF GPIO expander. The interrupt pin of GPIO expander PCA9535AHF is connected to ENET_TXD1 (GPIO1_IO29) in IMX6. I want to configure ENET_TXD1 (GPIO1_IO29) pin as interrupt (active low level-sensitive) . Please let me know how do i configure ENET_TXD1 (GPIO1_IO29) pin as interrupt.

Another question in board file how do i configure the "irq_base" value in pca953x_platform_data.

Thanks,

P.Ashok

Labels (5)
0 Kudos
Reply
0 Replies