GPIO and GPT Interrupt in u-boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPIO and GPT Interrupt in u-boot

1,982件の閲覧回数
erickang
Contributor II

Hi All,

I want to know how to use the interrupt in u-boot.

My development environment is like below,

- AP : i.MX257

- Board : i.MX25-PDK

- u-boot version : u-boot-2009.08

Actually I know the u-boot are using the polling mode in the all peripherals.

But I have to apply the interrupt mode for the GPIO and GPT.

Could you give me the method how to apply the interrupt mode in the u-boot?

Best Regards,

Eric.

ラベル(2)
0 件の賞賛
返信
1 返信

1,545件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Eric

suggest to look below

https://community.freescale.com/docs/DOC-100044

http://stackoverflow.com/questions/15829601/enabling-interrupts-in-u-boot-for-arm-cortex-a-9

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信