GPIO: Problem leak current while default power up

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

GPIO: Problem leak current while default power up

跳至解决方案
2,956 次查看
neusch
Contributor II

pastedImage_0.png

Have the i.MX6 only internal 100k pull-up or additional a diode ?

Is it the only way to solve the problem, by use a lot of Level-Shifter or Switch with trie-status ?

标签 (1)
0 项奖励
回复
1 解答
2,864 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Mathias

current through 1K should be limited to 1-2mA

Best regards

igor

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,864 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Mathias

i.MX6 has esd protection diodes on pads.

>Is it the only way to solve the problem, by use a lot of Level-Shifter or Switch with trie-status ?

also one can try to set external MCU outputs as logic "0".

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,864 次查看
neusch
Contributor II

Hi Igor,

that is correct. But i can't ensure this while power up.

pastedImage_1.png

Can you say something to this?

0 项奖励
回复
2,865 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Mathias

current through 1K should be limited to 1-2mA

Best regards

igor

0 项奖励
回复