GPIO: Problem leak current while default power up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPIO: Problem leak current while default power up

Jump to solution
2,977 Views
neusch
Contributor II

pastedImage_0.png

Have the i.MX6 only internal 100k pull-up or additional a diode ?

Is it the only way to solve the problem, by use a lot of Level-Shifter or Switch with trie-status ?

Labels (1)
0 Kudos
Reply
1 Solution
2,885 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mathias

current through 1K should be limited to 1-2mA

Best regards

igor

View solution in original post

0 Kudos
Reply
3 Replies
2,885 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mathias

i.MX6 has esd protection diodes on pads.

>Is it the only way to solve the problem, by use a lot of Level-Shifter or Switch with trie-status ?

also one can try to set external MCU outputs as logic "0".

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,885 Views
neusch
Contributor II

Hi Igor,

that is correct. But i can't ensure this while power up.

pastedImage_1.png

Can you say something to this?

0 Kudos
Reply
2,886 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mathias

current through 1K should be limited to 1-2mA

Best regards

igor

0 Kudos
Reply