GPIO DC/AC timing parameters in Schmitt trigger mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPIO DC/AC timing parameters in Schmitt trigger mode

2,683件の閲覧回数
ko-hey
Senior Contributor II

Hi all

I have question about GPIO specification.

I doubt that the DC/AC timing parameters are different.

Because the behavior is different in CMOS mode and Schmitt trigger mode in my board.

So I want to confirm the following.

1.

Does the DC parameter that is shown in P39 of IMX6SDLAEC is for CMOS mode ?

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLAEC.pdf

2.

Are there any different DC and AC parameter in CMOS mode and schmitt trigger mode ?

3.

In my understanding, i.MX becomes slower to recognize a "high" level in schmitt trigger mode than CMOS mode.

Because of the delay, is there possibility that i.MX can't latch the data correctly ?

ko-hey

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,526件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ko-hey

1. yes

2. with schmitt input hysteresis enabled, trigger may be later than

without hysteresis, because additional time is needed for signal

to reach hysteresis level. For example without hysteresis enabled

typical trigger level 0.5*OVDD, with hysteresis enabled it will be

0.5*OVDD + hysteresis value. According to Footnote 3 :

Hysteresis of 250 mV is guaranteed over all operating conditions when hysteresis is enabled.

3. yes this is correct understanding.

>Because of the delay, is there possibility that i.MX can't latch the data correctly ?

no.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,526件の閲覧回数
ko-hey
Senior Contributor II

Hi Igor

Let me confirm about question No.3.

You mean that i.MX may fail latching a data.

Is it correct ?

ko-hey

0 件の賞賛
返信

2,526件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ko-hey

no, meaning that i.MX will not fail latching a data.

Best regards

igor

0 件の賞賛
返信