GIC/PMU/RTC base physical address

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GIC/PMU/RTC base physical address

1,440件の閲覧回数
myungjinhwang
Contributor III

hi...........

I'm using IMX6_Sabrelite board.

I'd like to find some hardware physical address.

but I can not find GIC/PMU/RTC physical base address in the file.

where i can figure out ?

- i.MX 6Dual_6Quad Multimedia Applications Processor Reference Manual (REV B).pdf

- IMX6DQRM.pdf


i found that

     - L2C(0x00A02000)

     - SCU(0x00A00000)

     - GIC_CPU_BASE(0x00A00100)

     - GIC_DIST_BASE(0x00A01000)

     - IRAM(0x00900000)

please help me~~~

0 件の賞賛
返信
1 返信

1,288件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi MyungJin

for RTC one can look at Chapter 57 Secure Non-Volatile Storage (SNVS)

PMU -sect.50.7 PMU Memory Map/Register Definition IMX6DQRM

GIC is described in Chapter 4 Configuring the GIC Driver iMX6_Firmware_Guide.pdf

included in i.MX 6Series Platform SDK

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信